ConveyorStationFeatureBuilder Class¶
-
class
NXOpen.LineDesigner.
ConveyorStationFeatureBuilder
¶ Bases:
NXOpen.Builder
Represents a
LineDesigner.ConveyorStationFeature
builderTo create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateConveyorStationFeatureBuilder
Default values.
Property Value Capacity 0 ProcessTime 0 StationType Load New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Capacity | Returns or sets the capacity |
ProcessTime | Returns or sets the process time |
StationLocation | Returns or sets the station location |
StationName | Returns or sets the stattion name |
StationType | Returns or sets the station type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDescription | Returns the description @return |
GetObject | Returns the object currently being edited by this builder. |
SetDescription | Sets the description |
SetSECNode | |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ConveyorStationFeatureBuilderType Enumeration |
Property Detail¶
Capacity¶
-
ConveyorStationFeatureBuilder.
Capacity
¶ Returns or sets the capacity
-------------------------------------
Getter Method
Signature
Capacity()
Returns: Return type: float New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
Capacity(capacity)
Parameters: capacity (float) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ProcessTime¶
-
ConveyorStationFeatureBuilder.
ProcessTime
¶ Returns or sets the process time
-------------------------------------
Getter Method
Signature
ProcessTime()
Returns: Return type: float New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ProcessTime(processTime)
Parameters: processTime (float) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
StationLocation¶
-
ConveyorStationFeatureBuilder.
StationLocation
¶ Returns or sets the station location
-------------------------------------
Getter Method
Signature
StationLocation()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
StationLocation(stationLocation)
Parameters: stationLocation ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
StationName¶
-
ConveyorStationFeatureBuilder.
StationName
¶ Returns or sets the stattion name
-------------------------------------
Getter Method
Signature
StationName()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
StationName(stationName)
Parameters: stationName (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
StationType¶
-
ConveyorStationFeatureBuilder.
StationType
¶ Returns or sets the station type
-------------------------------------
Getter Method
Signature
StationType()
Returns: Return type: NXOpen.LineDesigner.ConveyorStationFeatureBuilderType
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
StationType(stationType)
Parameters: stationType ( NXOpen.LineDesigner.ConveyorStationFeatureBuilderType
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
GetDescription¶
-
ConveyorStationFeatureBuilder.
GetDescription
¶ Returns the description
Signature
GetDescription()
Returns: Return type: list of str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SetDescription¶
-
ConveyorStationFeatureBuilder.
SetDescription
¶ Sets the description
Signature
SetDescription(description)
Parameters: description (list of str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SetSECNode¶
-
ConveyorStationFeatureBuilder.
SetSECNode
¶ Signature
SetSECNode(secNode)
Parameters: secNode ( NXOpen.LineDesigner.DBConveyorNode
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Validate¶
-
ConveyorStationFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.