ConnectionCreatorBuilder Class¶
-
class
NXOpen.LineDesigner.
ConnectionCreatorBuilder
¶ Bases:
NXOpen.Builder
To create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateConnectionCreatorBuilder
Default values.
Property Value ConectionType Move New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ConectionType | Returns or sets the conection type |
SourceConnector | Returns the source connector |
Tag | Returns the Tag for this object. |
TargetConnector | Returns the target connector |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ConnectionCreatorBuilderConnectionType Enumeration |
Property Detail¶
ConectionType¶
-
ConnectionCreatorBuilder.
ConectionType
¶ Returns or sets the conection type
-------------------------------------
Getter Method
Signature
ConectionType()
Returns: Return type: NXOpen.LineDesigner.ConnectionCreatorBuilderConnectionType
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ConectionType(conectionType)
Parameters: conectionType ( NXOpen.LineDesigner.ConnectionCreatorBuilderConnectionType
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SourceConnector¶
-
ConnectionCreatorBuilder.
SourceConnector
¶ Returns the source connector
-------------------------------------
Getter Method
Signature
SourceConnector()
Returns: Return type: NXOpen.SelectPoint
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
TargetConnector¶
-
ConnectionCreatorBuilder.
TargetConnector
¶ Returns the target connector
-------------------------------------
Getter Method
Signature
TargetConnector()
Returns: Return type: NXOpen.SelectPoint
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
Validate¶
-
ConnectionCreatorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.