LightCollection Class¶
-
class
NXOpen.
LightCollection
¶ Bases:
object
Represents a collection of :py:class:`NXOpen.Light`s.
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.Light with the given identifier as recorded in a journal. |
SetLightIntensities | Modifies the intensities of a set of lights. |
Method Detail¶
FindObject¶
-
LightCollection.
FindObject
¶ Finds the
NXOpen.Light
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However, newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the Light to be found Returns: Light with this identifier Return type: NXOpen.Light
New in version NX4.0.0.
License requirements: None.
SetLightIntensities¶
-
LightCollection.
SetLightIntensities
¶ Modifies the intensities of a set of lights.
This is generally preferable to multiple consecutive invocations of
NXOpen.Light.Intensity
, as with this method the graphics screen is only updated once, while forNXOpen.Light.Intensity
it would be updated once per call.Signature
SetLightIntensities(lights, intensities)
Parameters: - lights (list of
NXOpen.Light
) – - intensities (list of float) –
New in version NX4.0.0.
License requirements: None.
- lights (list of