LicenseManager Class¶
-
class
NXOpen.
LicenseManager
¶ Bases:
object
Provides utility methods for managing licenses.
This class only manages the licenses that are used by the current NX Open application. If several applications are loaded in a session, each application will have its own independent license manager. It is possible for two applications to both reserve the same license. Although this will only reserve a single license from the FLEX server, the license will not be released to the server until both applications have released it.
As of NX6 the concept of User-Defined License Contexts has been introduced. This concept gives greater control of licensing of the application. To find out more about this topic, please reference the NXOpen Programmer’s Guide. All user-defined context names have a max length of 128 characters long consisting of only numbers and letters.
The main NX User Interface will also manage licenses independently. If an NX Open application releases the “solid_modeling” license, but the main NX UI is still using that license, then it will not be returned to the server.
Methods for this class use the license feature name, which can be found in the documentation for NX Open methods and properties. This is in the format <tt>License requirements: license feature name (“license description”)</tt>. For example, given <tt>License requirements: solid_modeling (“SOLIDS MODELING”)</tt>, then the license feature name, <tt>solid_modeling</tt> would be used.
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
GetReservedLicenses | Returns the licenses that are currently reserved against a context. |
Release | Release a license against the specified license context. |
ReleaseAll | Release all licenses against the specified license context. |
Reserve | Reserve a license against the specified license context. |
Method Detail¶
GetReservedLicenses¶
-
LicenseManager.
GetReservedLicenses
¶ Returns the licenses that are currently reserved against a context.
This method will also output the licenses reserved against the default context in the syslog.
Signature
GetReservedLicenses(contextName)
Parameters: contextName (str) – Name of context to release against. Will use the default context if None is specified. NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: list of str New in version NX6.0.0.
License requirements: None.
Release¶
-
LicenseManager.
Release
¶ Release a license against the specified license context.
Signature
Release(license, contextName)
Parameters: - license (str) – License feature name to be released NOTE: The full Unicode character set is not supported for this parameter.
- contextName (str) – Name of context to release license against. Will use the default context if None is specified. NOTE: The full Unicode character set is not supported for this parameter.
New in version NX6.0.0.
License requirements: None.
ReleaseAll¶
-
LicenseManager.
ReleaseAll
¶ Release all licenses against the specified license context.
If the context specified is a user-defined context it will be deleted.
Signature
ReleaseAll(contextName)
Parameters: contextName (str) – Name of context release to release. Will use the default context if None is specified. NOTE: The full Unicode character set is not supported for this parameter. New in version NX6.0.0.
License requirements: None.
Reserve¶
-
LicenseManager.
Reserve
¶ Reserve a license against the specified license context.
If the specified user-defined context does not already exist it will be created.
Signature
Reserve(license, contextName)
Parameters: - license (str) – License feature name to be reserved NOTE: The full Unicode character set is not supported for this parameter.
- contextName (str) – Name of context to reserve license against. Will use the default context if None is specified. NOTE: The full Unicode character set is not supported for this parameter.
New in version NX6.0.0.
License requirements: None.