InferredConstraintsBuilder Class¶
-
class
NXOpen.
InferredConstraintsBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.InferredConstraintsBuilder
To create a new instance of this class, use
NXOpen.SketchCollection.CreateInferredConstraintsBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Coincident | Returns or sets the coincident infer-constraint setting. |
Collinear | Returns or sets the collinear infer-constraint setting. |
Concentric | Returns or sets the concentric infer-constraint setting. |
DimensionalConstraint | Returns or sets the dimensional constraint infer-constraint setting. |
EqualLength | Returns or sets the equal length infer-constraint setting. |
EqualRadius | Returns or sets the equal radius infer-constraint setting. |
Horizontal | Returns or sets the horizontal infer-constraint setting. |
Midpoint | Returns or sets the midpoint infer-constraint setting. |
Parallel | Returns or sets the parallel infer-constraint setting. |
Perpendicular | Returns or sets the perpendicular infer-constraint setting. |
PointOnCurve | Returns or sets the point on curve infer-constraint setting. |
PointOnString | Returns or sets the point on string infer-constraint setting. |
Tag | Returns the Tag for this object. |
Tangent | Returns or sets the tangent infer-constraint setting. |
Vertical | Returns or sets the vertical infer-constraint setting. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetRules | Get the auto dimensioning rule list into an array @return |
SetRules | Set the auto dimensioning rule list to builder |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Coincident¶
-
InferredConstraintsBuilder.
Coincident
¶ Returns or sets the coincident infer-constraint setting.
If this constraint flag is switched ON, sketcher will create this constraint automatically for all coincident entities created after this command.
-------------------------------------
Getter Method
Signature
Coincident()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Coincident(coincident)
Parameters: coincident (bool) – New in version NX5.0.0.
License requirements: None.
Collinear¶
-
InferredConstraintsBuilder.
Collinear
¶ Returns or sets the collinear infer-constraint setting.
If this constraint flag is switched ON, sketcher will create this constraint automatically for all collinear entities created after this command.
-------------------------------------
Getter Method
Signature
Collinear()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Collinear(collinear)
Parameters: collinear (bool) – New in version NX5.0.0.
License requirements: None.
Concentric¶
-
InferredConstraintsBuilder.
Concentric
¶ Returns or sets the concentric infer-constraint setting.
If this constraint flag is switched ON, sketcher will create this constraint automatically for all concentric entities created after this command.
-------------------------------------
Getter Method
Signature
Concentric()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Concentric(concentric)
Parameters: concentric (bool) – New in version NX5.0.0.
License requirements: None.
DimensionalConstraint¶
-
InferredConstraintsBuilder.
DimensionalConstraint
¶ Returns or sets the dimensional constraint infer-constraint setting.
If this constraint flag is switched ON, sketcher will create dimensional constraints automatically for entities created after this command.
-------------------------------------
Getter Method
Signature
DimensionalConstraint()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DimensionalConstraint(dimensionalConstraint)
Parameters: dimensionalConstraint (bool) – New in version NX5.0.0.
License requirements: None.
EqualLength¶
-
InferredConstraintsBuilder.
EqualLength
¶ Returns or sets the equal length infer-constraint setting.
If this constraint flag is switched ON, sketcher will create this constraint automatically for all entities having equal length and created after this command.
-------------------------------------
Getter Method
Signature
EqualLength()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EqualLength(equalLength)
Parameters: equalLength (bool) – New in version NX5.0.0.
License requirements: None.
EqualRadius¶
-
InferredConstraintsBuilder.
EqualRadius
¶ Returns or sets the equal radius infer-constraint setting.
If this constraint flag is switched ON, sketcher will create this constraint automatically for all entities with equal radius and created after this command.
-------------------------------------
Getter Method
Signature
EqualRadius()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EqualRadius(equalRadius)
Parameters: equalRadius (bool) – New in version NX5.0.0.
License requirements: None.
Horizontal¶
-
InferredConstraintsBuilder.
Horizontal
¶ Returns or sets the horizontal infer-constraint setting.
If this constraint flag is switched ON, sketcher will create this constraint automatically for all horizonal entities created after this command.
-------------------------------------
Getter Method
Signature
Horizontal()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Horizontal(horizontal)
Parameters: horizontal (bool) – New in version NX5.0.0.
License requirements: None.
Midpoint¶
-
InferredConstraintsBuilder.
Midpoint
¶ Returns or sets the midpoint infer-constraint setting.
If this constraint flag is switched ON, sketcher will create this constraint automatically for all midpoints created after this command.
-------------------------------------
Getter Method
Signature
Midpoint()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Midpoint(midpoint)
Parameters: midpoint (bool) – New in version NX5.0.0.
License requirements: None.
Parallel¶
-
InferredConstraintsBuilder.
Parallel
¶ Returns or sets the parallel infer-constraint setting.
If this constraint flag is switched ON, sketcher will create this constraint automatically for all parallel entities created after this command.
-------------------------------------
Getter Method
Signature
Parallel()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Parallel(parallel)
Parameters: parallel (bool) – New in version NX5.0.0.
License requirements: None.
Perpendicular¶
-
InferredConstraintsBuilder.
Perpendicular
¶ Returns or sets the perpendicular infer-constraint setting.
If this constraint flag is switched ON, sketcher will create this constraint automatically for all perpendicular entities created after this command.
-------------------------------------
Getter Method
Signature
Perpendicular()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Perpendicular(perpendicular)
Parameters: perpendicular (bool) – New in version NX5.0.0.
License requirements: None.
PointOnCurve¶
-
InferredConstraintsBuilder.
PointOnCurve
¶ Returns or sets the point on curve infer-constraint setting.
If this constraint flag is switched ON, sketcher will create this constraint automatically for all points on curves created after this command.
-------------------------------------
Getter Method
Signature
PointOnCurve()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointOnCurve(pointOnCurve)
Parameters: pointOnCurve (bool) – New in version NX5.0.0.
License requirements: None.
PointOnString¶
-
InferredConstraintsBuilder.
PointOnString
¶ Returns or sets the point on string infer-constraint setting.
If this constraint flag is switched ON, sketcher will create this constraint automatically for all points on strings created after this command.
-------------------------------------
Getter Method
Signature
PointOnString()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointOnString(pointOnString)
Parameters: pointOnString (bool) – New in version NX5.0.0.
License requirements: None.
Tangent¶
-
InferredConstraintsBuilder.
Tangent
¶ Returns or sets the tangent infer-constraint setting.
If this constraint flag is switched ON, sketcher will create this constraint automatically for all tangent entities created after this command.
-------------------------------------
Getter Method
Signature
Tangent()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tangent(tangent)
Parameters: tangent (bool) – New in version NX5.0.0.
License requirements: None.
Vertical¶
-
InferredConstraintsBuilder.
Vertical
¶ Returns or sets the vertical infer-constraint setting.
If this constraint flag is switched ON, sketcher will create this constraint automatically for all vertical entities created after this command.
-------------------------------------
Getter Method
Signature
Vertical()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vertical(vertical)
Parameters: vertical (bool) – New in version NX5.0.0.
License requirements: None.
Method Detail¶
GetRules¶
-
InferredConstraintsBuilder.
GetRules
¶ Get the auto dimensioning rule list into an array
Signature
GetRules()
Returns: Return type: list of NXOpen.SketchAutoDimensioningRule
New in version NX7.5.0.
License requirements: None.
SetRules¶
-
InferredConstraintsBuilder.
SetRules
¶ Set the auto dimensioning rule list to builder
Signature
SetRules(rules)
Parameters: rules (list of NXOpen.SketchAutoDimensioningRule
) – Auto Dimension RulesNew in version NX7.5.0.
License requirements: None.
Validate¶
-
InferredConstraintsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.