SupportPlaneDataLockPlaneStatus Enumeration¶
NXOpen.GeometricUtilities.SupportPlaneData.LockPlaneStatus is an alias for NXOpen.GeometricUtilities.SupportPlaneDataLockPlaneStatus
-
class
NXOpen.GeometricUtilities.
SupportPlaneDataLockPlaneStatus
¶ Bases:
object
Represents support plane lock status for associative basic curves
Enum Members
Enum Member Enum Member Description No No LockAfterFirstConstraint Lock after first constraintAfterSecondConstraint Lock after second constraintAfterThirdConstraint Lock after third constraintAfterFirstAndSecondConstraint Lock after first and second constraintAfterFirstAndThirdConstraint Lock after first and third constraintAfterSecondAndThirdConstraint Lock after second and third constraintAfterAllConstraint Lock after all constraintLockExistingPlane Lock support plane using existing face or datumCenterPointDirection Lock support plane using center point and direction, this option should be used for Center Radius Arc only-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-