SpinePointDataParameterType Enumeration¶
NXOpen.GeometricUtilities.SpinePointData.ParameterType is an alias for NXOpen.GeometricUtilities.SpinePointDataParameterType
-
class
NXOpen.GeometricUtilities.
SpinePointDataParameterType
¶ Bases:
object
Parameter type
Enum Members
Enum Member Enum Member Description Normal Percent Parameter expressed as percent arc lengthLength Parameter expressed as arc length-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-