SpineDefinitionBuilder Class¶
-
class
NXOpen.GeometricUtilities.
SpineDefinitionBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Provides a spine definition for modeling operations
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Method | Returns or sets the method |
Section | Returns the section |
Tag | Returns the Tag for this object. |
Vector | Returns or sets the vector |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SpineDefinitionBuilderMethodOptions Enumeration | Options to define a spine |
Property Detail¶
Method¶
-
SpineDefinitionBuilder.
Method
¶ Returns or sets the method
-------------------------------------
Getter Method
Signature
Method()
Returns: Return type: NXOpen.GeometricUtilities.SpineDefinitionBuilderMethodOptions
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Method(method)
Parameters: method ( NXOpen.GeometricUtilities.SpineDefinitionBuilderMethodOptions
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Section¶
-
SpineDefinitionBuilder.
Section
¶ Returns the section
-------------------------------------
Getter Method
Signature
Section()
Returns: Return type: NXOpen.Section
New in version NX8.5.0.
License requirements: None.
Vector¶
-
SpineDefinitionBuilder.
Vector
¶ Returns or sets the vector
-------------------------------------
Getter Method
Signature
Vector()
Returns: Return type: NXOpen.Direction
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector(vector)
Parameters: vector ( NXOpen.Direction
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
SpineDefinitionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.