ShapeFrameBuilderAnchorAttachmentType Enumeration¶
NXOpen.GeometricUtilities.ShapeFrameBuilder.AnchorAttachmentType is an alias for NXOpen.GeometricUtilities.ShapeFrameBuilderAnchorAttachmentType
-
class
NXOpen.GeometricUtilities.
ShapeFrameBuilderAnchorAttachmentType
¶ Bases:
object
Represents the anchor attachment type
Enum Members
Enum Member Enum Member Description None Anchor is not attached to the frameCenter Anchor is attached to the center of the frameVertex1 Anchor is attached to the first vertex of the frameVertex2 Anchor is attached to the second vertex of the frameVertex3 Anchor is attached to the third vertex of the frameVertex4 Anchor is attached to the fourth vertex of the frame-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-