ScalingMethodBuilderScalingOptions Enumeration¶
NXOpen.GeometricUtilities.ScalingMethodBuilder.ScalingOptions is an alias for NXOpen.GeometricUtilities.ScalingMethodBuilderScalingOptions
-
class
NXOpen.GeometricUtilities.
ScalingMethodBuilderScalingOptions
¶ Bases:
object
This enum represents the scaling method option.
By default, it is set to Constant. Uniform and Lateral scaling options are invalid if only 1 guide is selected.
Enum Members
Enum Member Enum Member Description Constant ConstantByBlendingFunction Blending FunctionByAnotherCurve Another CurveByAPoint A PointByAreaLaw Area LawByPerimeterLaw Perimeter LawUniform Uniform, available only if 2 guides are selectedLateral Lateral, available only if 2 guides are selected-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-