SShapedLawBuilder Class¶
-
class
NXOpen.GeometricUtilities.
SShapedLawBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a s-shaped law.
This class represents
NXOpen.GeometricUtilities.LawBuilderType.SShaped
type of law inNXOpen.GeometricUtilities.LawBuilder
. Objects of classNXOpen.GeometricUtilities.OnPathDimWithValueBuilder
are used as law nodes inNXOpen.GeometricUtilities.SShapedLawBuilder
. Spine definition in this class is mandatory. The law nodes at start and end of the spine are fixed.New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
EndNode | Returns the end node |
SlopeNode | Returns the slope node |
Spine | Returns the Spine |
StartNode | Returns the start node |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
UpdateSpine | Update the builder based on current spine |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EndNode¶
-
SShapedLawBuilder.
EndNode
¶ Returns the end node
-------------------------------------
Getter Method
Signature
EndNode()
Returns: law node Return type: NXOpen.GeometricUtilities.OnPathDimWithValueBuilder
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
SlopeNode¶
-
SShapedLawBuilder.
SlopeNode
¶ Returns the slope node
-------------------------------------
Getter Method
Signature
SlopeNode()
Returns: law node Return type: NXOpen.GeometricUtilities.OnPathDimWithValueBuilder
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Spine¶
-
SShapedLawBuilder.
Spine
¶ Returns the Spine
-------------------------------------
Getter Method
Signature
Spine()
Returns: Section object representing spine Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
StartNode¶
-
SShapedLawBuilder.
StartNode
¶ Returns the start node
-------------------------------------
Getter Method
Signature
StartNode()
Returns: law node Return type: NXOpen.GeometricUtilities.OnPathDimWithValueBuilder
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
UpdateSpine¶
-
SShapedLawBuilder.
UpdateSpine
¶ Update the builder based on current spine
Signature
UpdateSpine()
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Validate¶
-
SShapedLawBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.