ReduceSurfaceRadiusBuilder Class¶
-
class
NXOpen.GeometricUtilities.
ReduceSurfaceRadiusBuilder
¶ Bases:
NXOpen.Builder
Reduce Surface Radius Builder of Geometric Utilities.
This builder’s Commit can produce more than one object, the GetCommittedObjects can be used to get the objects. To create a new instance of this class, use
NXOpen.GeometricUtilities.CAMDataPrepManager.CreateReduceSurfaceRadiusBuilder
Default values.
Property Value HighRadius 10.0 (millimeters part), 0.4 (inches part) LowRadius 0.5 (millimeters part), 0.02 (inches part) PercentReduction 100 ReduceValueType Percentage TargetReduction 0 ValueReduction 0.1 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Direction | Returns or sets the direction which specifies concave face respect to the body face normal |
FaceGroupList | Returns the list containing the face chains as input objects used to do reduction. |
HighRadius | Returns or sets the high radius which specifies lower limit to filter out all qualified faces |
IndexListItem | Returns or sets the index of list item |
LowRadius | Returns or sets the low radius which specifies lower limit to filter out all qualified faces |
OnPathDimEnd | Returns the end position of reduced sheet body |
OnPathDimStart | Returns the start position of reduced sheet body |
PercentReduction | Returns or sets the value of percentage reduction method |
PositionTolerance | Returns or sets the position tolerance between two faces connection |
ReduceValueType | Returns or sets the type of reduced value which results surface shape |
ReducedFaceType | Returns or sets the type of performing the radius reduction preview |
SelectChain | Returns the selected entities for performing the radius reduction operation, which selected by Select Faces by Chain and Single Selection |
SelectFace | Returns the selected entities for performing the radius reduction operation, which selected by Select Faces by Radius |
Tag | Returns the Tag for this object. |
TangentTolerance | Returns or sets the tangent tolerance between two faces connection |
TargetReduction | Returns or sets the target value method |
ValueReduction | Returns or sets the value of reduction value method |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ReduceSurfaceRadiusBuilderFaceSelectionSpecification Enumeration | Specify the face selection type. |
ReduceSurfaceRadiusBuilderReduceValueTypeSpecification Enumeration | Specify the reduction method. |
ReduceSurfaceRadiusBuilderReducedFaceTypeSpecification Enumeration | Specify three ways to do preview. |
Property Detail¶
Direction¶
-
ReduceSurfaceRadiusBuilder.
Direction
¶ Returns or sets the direction which specifies concave face respect to the body face normal
-------------------------------------
Getter Method
Signature
Direction()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Direction(direction)
Parameters: direction (bool) – New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”) OR die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
FaceGroupList¶
-
ReduceSurfaceRadiusBuilder.
FaceGroupList
¶ Returns the list containing the face chains as input objects used to do reduction.
-------------------------------------
Getter Method
Signature
FaceGroupList()
Returns: Return type: NXOpen.GeometricUtilities.ReduceSurfaceRadiusFaceGroupBuilderList
New in version NX9.0.0.
License requirements: None.
HighRadius¶
-
ReduceSurfaceRadiusBuilder.
HighRadius
¶ Returns or sets the high radius which specifies lower limit to filter out all qualified faces
-------------------------------------
Getter Method
Signature
HighRadius()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HighRadius(highRadius)
Parameters: highRadius (float) – New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”) OR die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
IndexListItem¶
-
ReduceSurfaceRadiusBuilder.
IndexListItem
¶ Returns or sets the index of list item
-------------------------------------
Getter Method
Signature
IndexListItem()
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IndexListItem(index)
Parameters: index (int) – New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”) OR die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
LowRadius¶
-
ReduceSurfaceRadiusBuilder.
LowRadius
¶ Returns or sets the low radius which specifies lower limit to filter out all qualified faces
-------------------------------------
Getter Method
Signature
LowRadius()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LowRadius(lowRadius)
Parameters: lowRadius (float) – New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”) OR die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OnPathDimEnd¶
-
ReduceSurfaceRadiusBuilder.
OnPathDimEnd
¶ Returns the end position of reduced sheet body
-------------------------------------
Getter Method
Signature
OnPathDimEnd()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX9.0.0.
License requirements: None.
OnPathDimStart¶
-
ReduceSurfaceRadiusBuilder.
OnPathDimStart
¶ Returns the start position of reduced sheet body
-------------------------------------
Getter Method
Signature
OnPathDimStart()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX9.0.0.
License requirements: None.
PercentReduction¶
-
ReduceSurfaceRadiusBuilder.
PercentReduction
¶ Returns or sets the value of percentage reduction method
-------------------------------------
Getter Method
Signature
PercentReduction()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PercentReduction(percentReduction)
Parameters: percentReduction (float) – New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”) OR die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
PositionTolerance¶
-
ReduceSurfaceRadiusBuilder.
PositionTolerance
¶ Returns or sets the position tolerance between two faces connection
-------------------------------------
Getter Method
Signature
PositionTolerance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PositionTolerance(positionTolerance)
Parameters: positionTolerance (float) – New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”) OR die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
ReduceValueType¶
-
ReduceSurfaceRadiusBuilder.
ReduceValueType
¶ Returns or sets the type of reduced value which results surface shape
-------------------------------------
Getter Method
Signature
ReduceValueType()
Returns: Return type: NXOpen.GeometricUtilities.ReduceSurfaceRadiusBuilderReduceValueTypeSpecification
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReduceValueType(reduceValueType)
Parameters: reduceValueType ( NXOpen.GeometricUtilities.ReduceSurfaceRadiusBuilderReduceValueTypeSpecification
) –New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”) OR die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
ReducedFaceType¶
-
ReduceSurfaceRadiusBuilder.
ReducedFaceType
¶ Returns or sets the type of performing the radius reduction preview
-------------------------------------
Getter Method
Signature
ReducedFaceType()
Returns: Return type: NXOpen.GeometricUtilities.ReduceSurfaceRadiusBuilderReducedFaceTypeSpecification
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReducedFaceType(reducedFaceType)
Parameters: reducedFaceType ( NXOpen.GeometricUtilities.ReduceSurfaceRadiusBuilderReducedFaceTypeSpecification
) –New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”) OR die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SelectChain¶
-
ReduceSurfaceRadiusBuilder.
SelectChain
¶ Returns the selected entities for performing the radius reduction operation, which selected by “Select Faces by Chain” and “Single Selection”
-------------------------------------
Getter Method
Signature
SelectChain()
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
SelectFace¶
-
ReduceSurfaceRadiusBuilder.
SelectFace
¶ Returns the selected entities for performing the radius reduction operation, which selected by “Select Faces by Radius”
-------------------------------------
Getter Method
Signature
SelectFace()
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
TangentTolerance¶
-
ReduceSurfaceRadiusBuilder.
TangentTolerance
¶ Returns or sets the tangent tolerance between two faces connection
-------------------------------------
Getter Method
Signature
TangentTolerance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TangentTolerance(tangentTolerance)
Parameters: tangentTolerance (float) – New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”) OR die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
TargetReduction¶
-
ReduceSurfaceRadiusBuilder.
TargetReduction
¶ Returns or sets the target value method
-------------------------------------
Getter Method
Signature
TargetReduction()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetReduction(targetReduction)
Parameters: targetReduction (float) – New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”) OR die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
ValueReduction¶
-
ReduceSurfaceRadiusBuilder.
ValueReduction
¶ Returns or sets the value of reduction value method
-------------------------------------
Getter Method
Signature
ValueReduction()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValueReduction(valueReduction)
Parameters: valueReduction (float) – New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”) OR die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
Validate¶
-
ReduceSurfaceRadiusBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.