PatternSpacingsListItem Class¶
-
class
NXOpen.GeometricUtilities.
PatternSpacingsListItem
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
one pattern spacing in the spacings list
To create a new instance of this class, use
NXOpen.GeometricUtilities.PatternSpacingsList.CreatePatternSpacingsListItem
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
SpacingExpression | Returns the spacing expression |
SpacingOnPath | Returns the spacing NXOpen.GeometricUtilities.OnPathDimensionBuilder |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SpacingExpression¶
-
PatternSpacingsListItem.
SpacingExpression
¶ Returns the spacing expression
-------------------------------------
Getter Method
Signature
SpacingExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
SpacingOnPath¶
-
PatternSpacingsListItem.
SpacingOnPath
¶ Returns the spacing
NXOpen.GeometricUtilities.OnPathDimensionBuilder
-------------------------------------
Getter Method
Signature
SpacingOnPath()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
PatternSpacingsListItem.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.