PatternOrientation Class¶
-
class
NXOpen.GeometricUtilities.
PatternOrientation
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
the pattern orientation definition.
Allows to specify an orientation option and corresponding entities. .. versionadded:: NX7.5.0
Properties¶
Property | Description |
---|---|
AlongOrientationOption | Returns or sets the orientationOption for Along pattern type |
AlongPathRotationAngle | Returns the along path rotation angle for the Along type pattern Normal to Path option. |
CircularOrientationOption | Returns or sets the orientationOption for Circular pattern type |
FollowFaceProjDirOption | Returns or sets the followFaceProjDirOption, an enum for follow face project direction. |
FollowFaceSelection | Returns the followFaceSelection, a sc collector to store selected faces. |
FollowFaceToggle | Returns or sets the followFaceToggle, a logical flag to indicate if the we need to modify the orientation to follow selected faces. |
FromCSYS | Returns or sets the fromCSYS, a CSYS for certain pattern type orientation need. |
GeneralOrientationOption | Returns or sets the orientationOption for General pattern type |
HelixOrientationOption | Returns or sets the orientationOption for Helix pattern type |
LinearOrientationOption | Returns or sets the orientationOption for Linear pattern type |
MirrorOrientationOption | Returns or sets the orientationOption for Mirror pattern type |
OrientationOption | Returns or sets the orientationOption for rectangular pattern type Note: this one does not have a straight forward replacement; Replacement based on pattern type: GeometricUtilities.PatternOrientation.LinearOrientationOption` GeometricUtilities.PatternOrientation.CircularOrientationOption` GeometricUtilities.PatternOrientation.AlongOrientationOption` GeometricUtilities.PatternOrientation.PolygonOrientationOption` GeometricUtilities.PatternOrientation.SpiralOrientationOption` GeometricUtilities.PatternOrientation.GeneralOrientationOption` GeometricUtilities.PatternOrientation.MirrorOrientationOption` GeometricUtilities.PatternOrientation.HelixOrientationOption` |
PolygonOrientationOption | Returns or sets the orientationOption for Polygon pattern type |
RepeatTransformSetting | Returns or sets the repeatTransformSetting, a logical flag to indicate if the we need to repeatedly apply the transform. |
SpiralOrientationOption | Returns or sets the orientationOption for Spiral pattern type |
Tag | Returns the Tag for this object. |
ToCSYS | Returns or sets the toCSYS, a CSYS for certain pattern type orientation need. |
UserDefinedProjDir | Returns or sets the userDefinedProjDir, a vector for user defined follow face project direction. |
VectorForAlong | Returns or sets the vectorForAlong, a vector for Along type orientation need. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PatternOrientationEnum Enumeration | pattern orientation options for all pattern types. |
PatternOrientationProjDirEnum Enumeration | pattern follow face project direction options available. |
Property Detail¶
AlongOrientationOption¶
-
PatternOrientation.
AlongOrientationOption
¶ Returns or sets the orientationOption for Along pattern type
-------------------------------------
Getter Method
Signature
AlongOrientationOption()
Returns: Return type: NXOpen.GeometricUtilities.PatternOrientationEnum
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlongOrientationOption(alongOrientationOption)
Parameters: alongOrientationOption ( NXOpen.GeometricUtilities.PatternOrientationEnum
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
AlongPathRotationAngle¶
-
PatternOrientation.
AlongPathRotationAngle
¶ Returns the along path rotation angle for the Along type pattern Normal to Path option.
-------------------------------------
Getter Method
Signature
AlongPathRotationAngle()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
CircularOrientationOption¶
-
PatternOrientation.
CircularOrientationOption
¶ Returns or sets the orientationOption for Circular pattern type
-------------------------------------
Getter Method
Signature
CircularOrientationOption()
Returns: Return type: NXOpen.GeometricUtilities.PatternOrientationEnum
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CircularOrientationOption(circularOrientationOption)
Parameters: circularOrientationOption ( NXOpen.GeometricUtilities.PatternOrientationEnum
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
FollowFaceProjDirOption¶
-
PatternOrientation.
FollowFaceProjDirOption
¶ Returns or sets the followFaceProjDirOption, an enum for follow face project direction.
-------------------------------------
Getter Method
Signature
FollowFaceProjDirOption()
Returns: Return type: NXOpen.GeometricUtilities.PatternOrientationProjDirEnum
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FollowFaceProjDirOption(followFaceProjDirOption)
Parameters: followFaceProjDirOption ( NXOpen.GeometricUtilities.PatternOrientationProjDirEnum
) –New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
FollowFaceSelection¶
-
PatternOrientation.
FollowFaceSelection
¶ Returns the followFaceSelection, a sc collector to store selected faces.
-------------------------------------
Getter Method
Signature
FollowFaceSelection()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
FollowFaceToggle¶
-
PatternOrientation.
FollowFaceToggle
¶ Returns or sets the followFaceToggle, a logical flag to indicate if the we need to modify the orientation to follow selected faces.
-------------------------------------
Getter Method
Signature
FollowFaceToggle()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FollowFaceToggle(followFaceToggle)
Parameters: followFaceToggle (bool) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
FromCSYS¶
-
PatternOrientation.
FromCSYS
¶ Returns or sets the fromCSYS, a CSYS for certain pattern type orientation need.
-------------------------------------
Getter Method
Signature
FromCSYS()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FromCSYS(fromCSYS)
Parameters: fromCSYS ( NXOpen.CoordinateSystem
) –New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
GeneralOrientationOption¶
-
PatternOrientation.
GeneralOrientationOption
¶ Returns or sets the orientationOption for General pattern type
-------------------------------------
Getter Method
Signature
GeneralOrientationOption()
Returns: Return type: NXOpen.GeometricUtilities.PatternOrientationEnum
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GeneralOrientationOption(generalOrientationOption)
Parameters: generalOrientationOption ( NXOpen.GeometricUtilities.PatternOrientationEnum
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
HelixOrientationOption¶
-
PatternOrientation.
HelixOrientationOption
¶ Returns or sets the orientationOption for Helix pattern type
-------------------------------------
Getter Method
Signature
HelixOrientationOption()
Returns: Return type: NXOpen.GeometricUtilities.PatternOrientationEnum
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HelixOrientationOption(helixOrientationOption)
Parameters: helixOrientationOption ( NXOpen.GeometricUtilities.PatternOrientationEnum
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
LinearOrientationOption¶
-
PatternOrientation.
LinearOrientationOption
¶ Returns or sets the orientationOption for Linear pattern type
-------------------------------------
Getter Method
Signature
LinearOrientationOption()
Returns: Return type: NXOpen.GeometricUtilities.PatternOrientationEnum
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinearOrientationOption(linearOrientationOption)
Parameters: linearOrientationOption ( NXOpen.GeometricUtilities.PatternOrientationEnum
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
MirrorOrientationOption¶
-
PatternOrientation.
MirrorOrientationOption
¶ Returns or sets the orientationOption for Mirror pattern type
-------------------------------------
Getter Method
Signature
MirrorOrientationOption()
Returns: Return type: NXOpen.GeometricUtilities.PatternOrientationEnum
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MirrorOrientationOption(mirrorOrientationOption)
Parameters: mirrorOrientationOption ( NXOpen.GeometricUtilities.PatternOrientationEnum
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
OrientationOption¶
-
PatternOrientation.
OrientationOption
¶ Returns or sets the orientationOption for rectangular pattern type Note: this one does not have a straight forward replacement; Replacement based on pattern type:
GeometricUtilities.PatternOrientation.LinearOrientationOption`
GeometricUtilities.PatternOrientation.CircularOrientationOption`
GeometricUtilities.PatternOrientation.AlongOrientationOption`
GeometricUtilities.PatternOrientation.PolygonOrientationOption`
GeometricUtilities.PatternOrientation.SpiralOrientationOption`
GeometricUtilities.PatternOrientation.GeneralOrientationOption`
GeometricUtilities.PatternOrientation.MirrorOrientationOption`
GeometricUtilities.PatternOrientation.HelixOrientationOption`
-------------------------------------
Getter Method
Signature
OrientationOption()
Returns: Return type: NXOpen.GeometricUtilities.PatternOrientationEnum
New in version NX7.5.0.
Deprecated since version NX8.0.0: The replacement function depends on the pattern type. See this method’s documentation for more detailed information.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationOption(orientationOption)
Parameters: orientationOption ( NXOpen.GeometricUtilities.PatternOrientationEnum
) –New in version NX7.5.0.
Deprecated since version NX8.0.0: The replacement function depends on the pattern type. See this method’s documentation for more detailed information.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
PolygonOrientationOption¶
-
PatternOrientation.
PolygonOrientationOption
¶ Returns or sets the orientationOption for Polygon pattern type
-------------------------------------
Getter Method
Signature
PolygonOrientationOption()
Returns: Return type: NXOpen.GeometricUtilities.PatternOrientationEnum
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PolygonOrientationOption(polygonOrientationOption)
Parameters: polygonOrientationOption ( NXOpen.GeometricUtilities.PatternOrientationEnum
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
RepeatTransformSetting¶
-
PatternOrientation.
RepeatTransformSetting
¶ Returns or sets the repeatTransformSetting, a logical flag to indicate if the we need to repeatedly apply the transform.
-------------------------------------
Getter Method
Signature
RepeatTransformSetting()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RepeatTransformSetting(repeatTransformSetting)
Parameters: repeatTransformSetting (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
SpiralOrientationOption¶
-
PatternOrientation.
SpiralOrientationOption
¶ Returns or sets the orientationOption for Spiral pattern type
-------------------------------------
Getter Method
Signature
SpiralOrientationOption()
Returns: Return type: NXOpen.GeometricUtilities.PatternOrientationEnum
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpiralOrientationOption(spiralOrientationOption)
Parameters: spiralOrientationOption ( NXOpen.GeometricUtilities.PatternOrientationEnum
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
ToCSYS¶
-
PatternOrientation.
ToCSYS
¶ Returns or sets the toCSYS, a CSYS for certain pattern type orientation need.
-------------------------------------
Getter Method
Signature
ToCSYS()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToCSYS(toCSYS)
Parameters: toCSYS ( NXOpen.CoordinateSystem
) –New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
UserDefinedProjDir¶
-
PatternOrientation.
UserDefinedProjDir
¶ Returns or sets the userDefinedProjDir, a vector for user defined follow face project direction.
-------------------------------------
Getter Method
Signature
UserDefinedProjDir()
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserDefinedProjDir(userDefinedProjDir)
Parameters: userDefinedProjDir ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
VectorForAlong¶
-
PatternOrientation.
VectorForAlong
¶ Returns or sets the vectorForAlong, a vector for Along type orientation need.
-------------------------------------
Getter Method
Signature
VectorForAlong()
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VectorForAlong(vectorForAlong)
Parameters: vectorForAlong ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
Method Detail¶
Validate¶
-
PatternOrientation.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.