PatternFillPatternFillOptions Enumeration¶
NXOpen.GeometricUtilities.PatternFill.PatternFillOptions is an alias for NXOpen.GeometricUtilities.PatternFillPatternFillOptions
-
class
NXOpen.GeometricUtilities.
PatternFillPatternFillOptions
¶ Bases:
object
This defines Fill Types
Enum Members
Enum Member Enum Member Description None no section is definedFillbyFace section is face-based, and for fill area.FillbyBoundary section is for fill area.ExcludeAreaOnly section is for exclude area only-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-