OrientXpressBuilderReference Enumeration¶
NXOpen.GeometricUtilities.OrientXpressBuilder.Reference is an alias for NXOpen.GeometricUtilities.OrientXpressBuilderReference
-
class
NXOpen.GeometricUtilities.
OrientXpressBuilderReference
¶ Bases:
object
the option for reference csys
Enum Members
Enum Member Enum Member Description AcsWorkPart Reference CSYS is absolute coordinate system in the work partAcsDisplayPart Reference CSYS is absolute coordinate system in the display partWcsWorkPart Reference CSYS is work coordinate system in the work partWcsDisplayPart Reference CSYS is work coordinate system in the display partCsys Reference CSYS is user specified coordinate systemFixed Reference CSYS is user defined coordinate systemProgramDefined Reference CSYS is application defined-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-