LocalUntrimBuilder Class¶
-
class
NXOpen.GeometricUtilities.
LocalUntrimBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.GeometricUtilities.LocalUntrimBuilder
builder.This builder is used to untrim and extend a sheet. To create a new instance of this class, use
NXOpen.GeometricUtilities.LocalUntrimManager.CreateBuilder
Default values.
Property Value EditCopy 0 UEndDistance.Value 0 (millimeters part), 0 (inches part) UStartDistance.Value 0 (millimeters part), 0 (inches part) VEndDistance.Value 0 (millimeters part), 0 (inches part) VStartDistance.Value 0 (millimeters part), 0 (inches part) New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
EdgeCollector | Returns the edges on the face to delete. |
EditCopy | Returns or sets the flag to indicate whether to edit a copied face or not. |
Face | Returns the tool object to split the target body. |
Tag | Returns the Tag for this object. |
UEndDistance | Returns the U end distance. |
UEndLimit | Returns the region limit of U end. |
UStartDistance | Returns the U start distance. |
UStartLimit | Returns the region limit of U start. |
VEndDistance | Returns the V end distance. |
VEndLimit | Returns the region limit of V end. |
VStartDistance | Returns the V start distance. |
VStartLimit | Returns the region limit of V start. |
Methods¶
Method | Description |
---|---|
CleanUpFeaturesCreated | Cleans up the features created by the selecting face call back. |
Commit | Commits any edits that have been applied to the builder. |
CreateCopyFace | Creates the extracted face when the flag of Edit a Copy is turned on or a solid body face is selected. |
CreateProductBoundingBox | Creates the product initial bounding box. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetCurrentFeature | Records the current feature before constructing the dialog. |
SetOriginalFace | Sets the originally selected face. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateBoundingBox | Updates the bounding box when changing the distance value. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EdgeCollector¶
-
LocalUntrimBuilder.
EdgeCollector
¶ Returns the edges on the face to delete.
-------------------------------------
Getter Method
Signature
EdgeCollector()
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
EditCopy¶
-
LocalUntrimBuilder.
EditCopy
¶ Returns or sets the flag to indicate whether to edit a copied face or not.
-------------------------------------
Getter Method
Signature
EditCopy()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EditCopy(editCopy)
Parameters: editCopy (bool) – New in version NX9.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”) OR nx_freeform_2 (“advanced freeform modeling”)
Face¶
-
LocalUntrimBuilder.
Face
¶ Returns the tool object to split the target body.
-------------------------------------
Getter Method
Signature
Face()
Returns: Return type: NXOpen.SelectFace
New in version NX9.0.0.
License requirements: None.
UEndDistance¶
-
LocalUntrimBuilder.
UEndDistance
¶ Returns the U end distance.
-------------------------------------
Getter Method
Signature
UEndDistance()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
UEndLimit¶
-
LocalUntrimBuilder.
UEndLimit
¶ Returns the region limit of U end.
-------------------------------------
Getter Method
Signature
UEndLimit()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX9.0.0.
License requirements: None.
UStartDistance¶
-
LocalUntrimBuilder.
UStartDistance
¶ Returns the U start distance.
-------------------------------------
Getter Method
Signature
UStartDistance()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
UStartLimit¶
-
LocalUntrimBuilder.
UStartLimit
¶ Returns the region limit of U start.
-------------------------------------
Getter Method
Signature
UStartLimit()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX9.0.0.
License requirements: None.
VEndDistance¶
-
LocalUntrimBuilder.
VEndDistance
¶ Returns the V end distance.
-------------------------------------
Getter Method
Signature
VEndDistance()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
VEndLimit¶
-
LocalUntrimBuilder.
VEndLimit
¶ Returns the region limit of V end.
-------------------------------------
Getter Method
Signature
VEndLimit()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX9.0.0.
License requirements: None.
VStartDistance¶
-
LocalUntrimBuilder.
VStartDistance
¶ Returns the V start distance.
-------------------------------------
Getter Method
Signature
VStartDistance()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
VStartLimit¶
-
LocalUntrimBuilder.
VStartLimit
¶ Returns the region limit of V start.
-------------------------------------
Getter Method
Signature
VStartLimit()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
CleanUpFeaturesCreated¶
-
LocalUntrimBuilder.
CleanUpFeaturesCreated
¶ Cleans up the features created by the selecting face call back.
Signature
CleanUpFeaturesCreated()
New in version NX9.0.0.
License requirements: None.
CreateCopyFace¶
-
LocalUntrimBuilder.
CreateCopyFace
¶ Creates the extracted face when the flag of Edit a Copy is turned on or a solid body face is selected.
Signature
CreateCopyFace()
New in version NX9.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”) OR nx_freeform_2 (“advanced freeform modeling”)
CreateProductBoundingBox¶
-
LocalUntrimBuilder.
CreateProductBoundingBox
¶ Creates the product initial bounding box.
Signature
CreateProductBoundingBox()
New in version NX9.0.0.
License requirements: None.
SetCurrentFeature¶
-
LocalUntrimBuilder.
SetCurrentFeature
¶ Records the current feature before constructing the dialog.
Signature
SetCurrentFeature(object)
Parameters: object ( NXOpen.Features.Feature
) –New in version NX9.0.0.
License requirements: None.
SetOriginalFace¶
-
LocalUntrimBuilder.
SetOriginalFace
¶ Sets the originally selected face.
Signature
SetOriginalFace(originalFace)
Parameters: originalFace ( NXOpen.Face
) –New in version NX9.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”) OR nx_freeform_2 (“advanced freeform modeling”)
UpdateBoundingBox¶
-
LocalUntrimBuilder.
UpdateBoundingBox
¶ Updates the bounding box when changing the distance value.
Signature
UpdateBoundingBox()
New in version NX9.0.0.
License requirements: None.
Validate¶
-
LocalUntrimBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.