LawBuilderRetainLawCurveOption Enumeration¶
NXOpen.GeometricUtilities.LawBuilder.RetainLawCurveOption is an alias for NXOpen.GeometricUtilities.LawBuilderRetainLawCurveOption
-
class
NXOpen.GeometricUtilities.
LawBuilderRetainLawCurveOption
¶ Bases:
object
Describes the option on whether to retain the original profile.
Enum Members
Enum Member Enum Member Description KeepOriginal Keeps the original profile as it is during edit pre NX3 parmsReplace Deletes the old profile, so that user has to select new one during edit pre NX3 parms-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-