InstanceEditedExpressionItem Class¶
-
class
NXOpen.GeometricUtilities.
InstanceEditedExpressionItem
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
edited value of one master expression of the input object(s) being patterned.
To create a new instance of this class, use
NXOpen.GeometricUtilities.InstanceEditedExpressionsList.EditInstanceExpression
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
MasterExpression | Returns the master expression |
Tag | Returns the Tag for this object. |
ValueExpression | Returns the edited value expression for the master expression |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
MasterExpression¶
-
InstanceEditedExpressionItem.
MasterExpression
¶ Returns the master expression
-------------------------------------
Getter Method
Signature
MasterExpression()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
ValueExpression¶
-
InstanceEditedExpressionItem.
ValueExpression
¶ Returns the edited value expression for the master expression
-------------------------------------
Getter Method
Signature
ValueExpression()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
InstanceEditedExpressionItem.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.