FtmTransformPointsBuilder Class¶
-
class
NXOpen.GeometricUtilities.
FtmTransformPointsBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.GeometricUtilities.FtmTransformPointsBuilder
builderTo create a new instance of this class, use
NXOpen.GeometricUtilities.OmnicadManager.CreateFtmTransformPointsBuilder
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
TransformEndPoint | Returns or sets the end point that defines the end or target point constraint on the product shape |
TransformStartPoint | Returns or sets the start point that defines the starting point constraint on the product shape |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
TransformEndPoint¶
-
FtmTransformPointsBuilder.
TransformEndPoint
¶ Returns or sets the end point that defines the end or target point constraint on the product shape
-------------------------------------
Getter Method
Signature
TransformEndPoint()
Returns: Return type: NXOpen.Point
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransformEndPoint(transformEndPoint)
Parameters: transformEndPoint ( NXOpen.Point
) –New in version NX10.0.0.
License requirements: None.
TransformStartPoint¶
-
FtmTransformPointsBuilder.
TransformStartPoint
¶ Returns or sets the start point that defines the starting point constraint on the product shape
-------------------------------------
Getter Method
Signature
TransformStartPoint()
Returns: Return type: NXOpen.Point
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransformStartPoint(transformStartPoint)
Parameters: transformStartPoint ( NXOpen.Point
) –New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
FtmTransformPointsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.