FtmFixedCurvesBuilder Class¶
-
class
NXOpen.GeometricUtilities.
FtmFixedCurvesBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.GeometricUtilities.FtmFixedCurvesBuilder
builderTo create a new instance of this class, use
NXOpen.GeometricUtilities.OmnicadManager.CreateFtmFixedCurvesBuilder
Default values.
Property Value FixedCurvesContinuity G0 New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
FixedCurves | Returns the fixed curves that define the fixed constraints on the product shape |
FixedCurvesContinuity | Returns or sets the continuity option for the fixed curves used in the transformation or morphing calculations |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FtmFixedCurvesBuilderFixedCurvesContinuityType Enumeration | Fixed curves continuity type |
Property Detail¶
FixedCurves¶
-
FtmFixedCurvesBuilder.
FixedCurves
¶ Returns the fixed curves that define the fixed constraints on the product shape
-------------------------------------
Getter Method
Signature
FixedCurves()
Returns: Return type: NXOpen.Section
New in version NX10.0.0.
License requirements: None.
FixedCurvesContinuity¶
-
FtmFixedCurvesBuilder.
FixedCurvesContinuity
¶ Returns or sets the continuity option for the fixed curves used in the transformation or morphing calculations
-------------------------------------
Getter Method
Signature
FixedCurvesContinuity()
Returns: Return type: NXOpen.GeometricUtilities.FtmFixedCurvesBuilderFixedCurvesContinuityType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FixedCurvesContinuity(fixedCurvesContinuity)
Parameters: fixedCurvesContinuity ( NXOpen.GeometricUtilities.FtmFixedCurvesBuilderFixedCurvesContinuityType
) –New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
FtmFixedCurvesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.