FlowDirection Class¶
-
class
NXOpen.GeometricUtilities.
FlowDirection
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.FlowDirection
Allows user to specify different flow direction to control output surface shape.New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
FlowDirectionType | Returns or sets the flow direction type. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FlowDirectionType Enumeration | flow direction type. |
Property Detail¶
FlowDirectionType¶
-
FlowDirection.
FlowDirectionType
¶ Returns or sets the flow direction type.
-------------------------------------
Getter Method
Signature
FlowDirectionType()
Returns: Return type: NXOpen.GeometricUtilities.FlowDirectionType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlowDirectionType(flowDirectionType)
Parameters: flowDirectionType ( NXOpen.GeometricUtilities.FlowDirectionType
) –New in version NX5.0.0.
License requirements: nx_freeform_1 (“basic freeform modeling”)
Method Detail¶
Validate¶
-
FlowDirection.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.