EnumTestCurves Enumeration¶
NXOpen.GeometricUtilities.EnumTest.Curves is an alias for NXOpen.GeometricUtilities.EnumTestCurves
-
class
NXOpen.GeometricUtilities.
EnumTestCurves
¶ Bases:
object
Curves are important
Enum Members
Enum Member Enum Member Description Line the granddaddy of all curvesArc arcs are always jealous of lines’ notorietyCircle where do they start? The answer blows in the wind-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-