EnumTestAnimals Enumeration¶
NXOpen.GeometricUtilities.EnumTest.Animals is an alias for NXOpen.GeometricUtilities.EnumTestAnimals
-
class
NXOpen.GeometricUtilities.
EnumTestAnimals
¶ Bases:
object
Animals are healthy and taste good
Enum Members
Enum Member Enum Member Description Pika rabbit with mouse earsAardvark no better animal nameHippo Hippos are bigSnake Snakes are not really slimey-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-