DraftVariableAngleData Class¶
-
class
NXOpen.GeometricUtilities.
DraftVariableAngleData
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents data containing variable angle draft point data objects
This class will not be created by the user.
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
AddDraftPoints | Adds NXOpen.GeometricUtilities.DraftPointData objects |
GetDraftPoints | Returns NXOpen.GeometricUtilities.DraftPointData objects @return Array of DraftPointData Objects |
GetNumberOfDraftPoints | Returns number of NXOpen.GeometricUtilities.DraftPointData objects @return Number of DraftPointData Objects |
RemoveDraftPoints | Removes NXOpen.GeometricUtilities.DraftPointData objects |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
AddDraftPoints¶
-
DraftVariableAngleData.
AddDraftPoints
¶ Adds
NXOpen.GeometricUtilities.DraftPointData
objectsSignature
AddDraftPoints(points)
Parameters: points (list of NXOpen.GeometricUtilities.DraftPointData
) – Array of DraftPointData ObjectsNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetDraftPoints¶
-
DraftVariableAngleData.
GetDraftPoints
¶ Returns
NXOpen.GeometricUtilities.DraftPointData
objectsSignature
GetDraftPoints()
Returns: Array of DraftPointData Objects Return type: list of NXOpen.GeometricUtilities.DraftPointData
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetNumberOfDraftPoints¶
-
DraftVariableAngleData.
GetNumberOfDraftPoints
¶ Returns number of
NXOpen.GeometricUtilities.DraftPointData
objectsSignature
GetNumberOfDraftPoints()
Returns: Number of DraftPointData Objects Return type: int New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RemoveDraftPoints¶
-
DraftVariableAngleData.
RemoveDraftPoints
¶ Removes
NXOpen.GeometricUtilities.DraftPointData
objectsSignature
RemoveDraftPoints(points)
Parameters: points (list of NXOpen.GeometricUtilities.DraftPointData
) – Array of DraftPointData ObjectsNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
DraftVariableAngleData.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.