CurveFitJoin Class¶
-
class
NXOpen.GeometricUtilities.
CurveFitJoin
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the curve fit join data
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CurveFitOptions | Returns the curve fit options |
CurveJoinMethod | Returns or sets the curve join method |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CurveFitJoinJoinMethod Enumeration | Represents the curve join method |
Property Detail¶
CurveFitOptions¶
-
CurveFitJoin.
CurveFitOptions
¶ Returns the curve fit options
-------------------------------------
Getter Method
Signature
CurveFitOptions()
Returns: Return type: NXOpen.GeometricUtilities.CurveFitOptions
New in version NX5.0.0.
License requirements: None.
CurveJoinMethod¶
-
CurveFitJoin.
CurveJoinMethod
¶ Returns or sets the curve join method
-------------------------------------
Getter Method
Signature
CurveJoinMethod()
Returns: curve fit method Return type: NXOpen.GeometricUtilities.CurveFitJoinJoinMethod
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
CurveJoinMethod(curveJoinMethod)
Parameters: curveJoinMethod ( NXOpen.GeometricUtilities.CurveFitJoinJoinMethod
) – curve fit methodNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
CurveFitJoin.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.