ColorCodedRegionBuilder Class¶
-
class
NXOpen.GeometricUtilities.
ColorCodedRegionBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.ColorCodedRegionBuilder
.The Color Coded Region block allows the user to select color coded regions of facet bodies . .. versionadded:: NX10.0.0
Properties¶
Property | Description |
---|---|
AllSameColor | Returns or sets the option to select all regions of the same color |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
BuildColoredRegion | Build Colored Region |
DeselectColoredRegion | Deselect Colored Region |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AllSameColor¶
-
ColorCodedRegionBuilder.
AllSameColor
¶ Returns or sets the option to select all regions of the same color
-------------------------------------
Getter Method
Signature
AllSameColor()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AllSameColor(allSameColor)
Parameters: allSameColor (bool) – New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
BuildColoredRegion¶
-
ColorCodedRegionBuilder.
BuildColoredRegion
¶ Build Colored Region
Signature
BuildColoredRegion(facetBody, facetId, localVertexId)
Parameters: - facetBody (
NXOpen.Facet.FacetedBody
) – target facet body - facetId (int) – picked facet ID
- localVertexId (int) – loccal vertex id of the triangle
New in version NX10.0.0.
License requirements: None.
- facetBody (
DeselectColoredRegion¶
-
ColorCodedRegionBuilder.
DeselectColoredRegion
¶ Deselect Colored Region
Signature
DeselectColoredRegion(objIndex)
Parameters: objIndex (int) – colored object to be deselected New in version NX10.0.0.
License requirements: None.
Validate¶
-
ColorCodedRegionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.