BoundaryDefinitionBuilder Class

class NXOpen.GeometricUtilities.BoundaryDefinitionBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.GeometricUtilities.BoundaryDefinitionBuilder.

A boundary definition is a collection of ordered points which can be imagined to be connected by a polyline indicating a boundary. Any point in the collection can be marked as a key point. Marking some points as key points helps to delete part of the boundary efficiently. All the points in a boundary definition are co-planar. A depth value can be specified to define a 3D boundary equivalent to an extrusion. .. versionadded:: NX7.5.0

Properties

Property Description
Depth Returns the region depth
Tag Returns the Tag for this object.

Methods

Method Description
AppendPoint Appends a point to the boundary definition
Close Closes the boundary by appending start point at the end of boundary definition @return
DeleteAll Deletes all the points in the boundary definition
DeleteLastKeyPoint Deletes last key point and all the points from last key point up to and excluding its previous key point
GetPoints Queries all the boundary definition points @return
SetPlaneNormal Sets normal of the plane in which boundary is defined
Translate Translates the boundary from its current position using the direction and the magnitude of a vector.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

Depth

BoundaryDefinitionBuilder.Depth

Returns the region depth

-------------------------------------

Getter Method

Signature Depth()

Returns:
Return type:NXOpen.Expression

New in version NX7.5.0.

License requirements: None.

Method Detail

AppendPoint

BoundaryDefinitionBuilder.AppendPoint

Appends a point to the boundary definition

Signature AppendPoint(point, isKeyPoint)

Parameters:
  • point (NXOpen.Point3d) – Point to append
  • isKeyPoint (bool) – Flag indicating if point is a key point

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

Close

BoundaryDefinitionBuilder.Close

Closes the boundary by appending start point at the end of boundary definition

Signature Close()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

DeleteAll

BoundaryDefinitionBuilder.DeleteAll

Deletes all the points in the boundary definition

Signature DeleteAll()

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

DeleteLastKeyPoint

BoundaryDefinitionBuilder.DeleteLastKeyPoint

Deletes last key point and all the points from last key point up to and excluding its previous key point

Signature DeleteLastKeyPoint()

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

GetPoints

BoundaryDefinitionBuilder.GetPoints

Queries all the boundary definition points

Signature GetPoints()

Returns:
Return type:list of NXOpen.Point3d

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

SetPlaneNormal

BoundaryDefinitionBuilder.SetPlaneNormal

Sets normal of the plane in which boundary is defined

Signature SetPlaneNormal(direction)

Parameters:direction (NXOpen.Vector3d) –

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

Translate

BoundaryDefinitionBuilder.Translate

Translates the boundary from its current position using the direction and the magnitude of a vector.

Signature Translate(vector)

Parameters:vector (NXOpen.Vector3d) –

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

Validate

BoundaryDefinitionBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.