BooleanToolBuilder Class¶
-
class
NXOpen.GeometricUtilities.
BooleanToolBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
a class which defines boolean tool builder.
It provides four types of * tool creation methods viz. a set of existing faces or datum planes, a new plane * created on the fly (FacePlaneToolBuilder), extrude or revolve sheet bodies created on the fly by * a given section and direction (ExtrudeRevolveToolBuilder).
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ExtrudeRevolveTool | Returns the ExtrudeRevolveTool builder. |
FacePlaneTool | Returns the FacePlaneTool Builder. |
ReverseDirection | Returns or sets the boolean tool reverse direction option |
Tag | Returns the Tag for this object. |
ToolOption | Returns or sets the boolean tool option |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BooleanToolBuilderBooleanToolType Enumeration | the boolean tool created options |
Property Detail¶
ExtrudeRevolveTool¶
-
BooleanToolBuilder.
ExtrudeRevolveTool
¶ Returns the ExtrudeRevolveTool builder.
Through this tool, the extrude * or revolve created on the fly can be queried
-------------------------------------
Getter Method
Signature
ExtrudeRevolveTool()
Returns: Return type: NXOpen.GeometricUtilities.ExtrudeRevolveToolBuilder
New in version NX6.0.0.
License requirements: None.
FacePlaneTool¶
-
BooleanToolBuilder.
FacePlaneTool
¶ Returns the FacePlaneTool Builder.
Through this tool, the sets of tool faces/datum planes or * new plane created on the fly can be queried
-------------------------------------
Getter Method
Signature
FacePlaneTool()
Returns: Return type: NXOpen.GeometricUtilities.FacePlaneToolBuilder
New in version NX6.0.0.
License requirements: None.
ReverseDirection¶
-
BooleanToolBuilder.
ReverseDirection
¶ Returns or sets the boolean tool reverse direction option
-------------------------------------
Getter Method
Signature
ReverseDirection()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection(reverseDirection)
Parameters: reverseDirection (bool) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ToolOption¶
-
BooleanToolBuilder.
ToolOption
¶ Returns or sets the boolean tool option
-------------------------------------
Getter Method
Signature
ToolOption()
Returns: Return type: NXOpen.GeometricUtilities.BooleanToolBuilderBooleanToolType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolOption(toolOption)
Parameters: toolOption ( NXOpen.GeometricUtilities.BooleanToolBuilderBooleanToolType
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
BooleanToolBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.