SolidDensity Class¶
-
class
NXOpen.GeometricAnalysis.
SolidDensity
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.GeometricAnalysis.SolidDensity
To create a new instance of this class, use
NXOpen.GeometricAnalysis.AnalysisManager.CreateSolidDensityObject
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Density | Returns or sets the Solid Density. |
Solids | Returns the solids to set density for |
Tag | Returns the Tag for this object. |
Units | Returns or sets the density units for NXOpen.GeometricAnalysis.SolidDensity . |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SolidDensityUnitsType Enumeration | Types of units for solid density |
Property Detail¶
Density¶
-
SolidDensity.
Density
¶ Returns or sets the Solid Density.
NXOpen.GeometricAnalysis.SolidDensity.Units
must be specified before specifying the density. WhenNXOpen.GeometricAnalysis.SolidDensity.Units
is changed,NXOpen.GeometricAnalysis.SolidDensity.Density
value is recomputed to reflect the change in units. SetNXOpen.GeometricAnalysis.SolidDensity.Units
first, thenNXOpen.GeometricAnalysis.SolidDensity.Density
to set specify the density along with its units.-------------------------------------
Getter Method
Signature
Density()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Density(density)
Parameters: density (float) – New in version NX5.0.0.
License requirements: None.
Solids¶
-
SolidDensity.
Solids
¶ Returns the solids to set density for
-------------------------------------
Getter Method
Signature
Solids()
Returns: Return type: NXOpen.SelectObjectList
New in version NX5.0.0.
License requirements: None.
Units¶
-
SolidDensity.
Units
¶ Returns or sets the density units for
NXOpen.GeometricAnalysis.SolidDensity
.When
NXOpen.GeometricAnalysis.SolidDensity.Units
is changed,NXOpen.GeometricAnalysis.SolidDensity.Density
value is recomputed to reflect the change in units. SetNXOpen.GeometricAnalysis.SolidDensity.Units
first, thenNXOpen.GeometricAnalysis.SolidDensity.Density
to set specify the density with units.-------------------------------------
Getter Method
Signature
Units()
Returns: Return type: NXOpen.GeometricAnalysis.SolidDensityUnitsType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Units(units)
Parameters: units ( NXOpen.GeometricAnalysis.SolidDensityUnitsType
) – Type of UnitsNew in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SolidDensity.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.