SectionAnalysisExBuilderPlacementType Enumeration¶
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder.PlacementType is an alias for NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderPlacementType
-
class
NXOpen.GeometricAnalysis.SectionAnalysis.
SectionAnalysisExBuilderPlacementType
¶ Bases:
object
The types of the section placement
Enum Members
Enum Member Enum Member Description Uniform Uniformly distributedThroughPoints Through the specified pointsBetweenPoints Distributed between two specified pointsInteractive Interactively specified-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-