QuadrilateralGridBuilder Class¶
-
class
NXOpen.GeometricAnalysis.SectionAnalysis.
QuadrilateralGridBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the quadrilateral grid section specifications for a
GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilder
.Only used when type is
GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilderTypes.Quadrilateral
.New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
QuadrilateralFrame | Returns the quadrilateral frame |
Spacing | Returns the spacing specification for the quadrilateral grid |
SpecifiedPlane | Returns the user specified section plane |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
QuadrilateralFrame¶
-
QuadrilateralGridBuilder.
QuadrilateralFrame
¶ Returns the quadrilateral frame
-------------------------------------
Getter Method
Signature
QuadrilateralFrame()
Returns: Return type: NXOpen.GeometricUtilities.QuadrilateralFrameBuilder
New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Spacing¶
-
QuadrilateralGridBuilder.
Spacing
¶ Returns the spacing specification for the quadrilateral grid
-------------------------------------
Getter Method
Signature
Spacing()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.GridSpacingBuilder
New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
SpecifiedPlane¶
-
QuadrilateralGridBuilder.
SpecifiedPlane
¶ Returns the user specified section plane
-------------------------------------
Getter Method
Signature
SpecifiedPlane()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.SectionPlaneBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
QuadrilateralGridBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.