CircularGridBuilder Class¶
-
class
NXOpen.GeometricAnalysis.SectionAnalysis.
CircularGridBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the circular grid section specifications for a
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilder
.Only used when type is
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilderTypes.Circular
.New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CircularFrame | Returns the circular frame |
Spacing | Returns the spacing specification for the circular grid |
SpecifiedPlane | Returns the user specified section plane |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CircularFrame¶
-
CircularGridBuilder.
CircularFrame
¶ Returns the circular frame
-------------------------------------
Getter Method
Signature
CircularFrame()
Returns: Return type: NXOpen.GeometricUtilities.CircularFrameBuilder
New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Spacing¶
-
CircularGridBuilder.
Spacing
¶ Returns the spacing specification for the circular grid
-------------------------------------
Getter Method
Signature
Spacing()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.GridSpacingBuilder
New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
SpecifiedPlane¶
-
CircularGridBuilder.
SpecifiedPlane
¶ Returns the user specified section plane
-------------------------------------
Getter Method
Signature
SpecifiedPlane()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.SectionPlaneBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
CircularGridBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.