LocalRadiusAnalysisBuilder Class¶
-
class
NXOpen.GeometricAnalysis.
LocalRadiusAnalysisBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.GeometricAnalysis.LocalRadiusAnalysis
builderTo create a new instance of this class, use
NXOpen.GeometricAnalysis.AnalysisObjectCollection.CreateLocalRadiusAnalysisBuilder
Default values.
Property Value VisibilityCoordinates 0 VisibilityMaxRadius 0 VisibilityMinMaxRadiusTangent 0 VisibilityMinRadius 1 VisibilityRadius 1 VisibilityURadius 0 VisibilityUV 0 VisibilityUVTangent 0 VisibilityVRadius 0 New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
SelectionPoint | Returns the selection point |
Tag | Returns the Tag for this object. |
VisibilityCoordinates | Returns or sets the toggle coordinates |
VisibilityMaxRadius | Returns or sets the toggle max radius show |
VisibilityMinMaxRadiusTangent | Returns or sets the toggle min radius tangent |
VisibilityMinRadius | Returns or sets the toggle min radius show |
VisibilityRadius | Returns or sets the toggle radius show |
VisibilityURadius | Returns or sets the toggle uradius show |
VisibilityUV | Returns or sets the toggle uv |
VisibilityUVTangent | Returns or sets the toggle max radius tangent |
VisibilityVRadius | Returns or sets the toggle vradius show |
Methods¶
Method | Description |
---|---|
ButtonOpenInformationWindow | TODO: fill in a description for this |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SelectionPoint¶
-
LocalRadiusAnalysisBuilder.
SelectionPoint
¶ Returns the selection point
-------------------------------------
Getter Method
Signature
SelectionPoint()
Returns: Return type: NXOpen.Features.GeometricConstraintDataManager
New in version NX8.5.0.
License requirements: None.
VisibilityCoordinates¶
-
LocalRadiusAnalysisBuilder.
VisibilityCoordinates
¶ Returns or sets the toggle coordinates
-------------------------------------
Getter Method
Signature
VisibilityCoordinates()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibilityCoordinates(visibilityCoordinates)
Parameters: visibilityCoordinates (bool) – New in version NX8.5.0.
License requirements: None.
VisibilityMaxRadius¶
-
LocalRadiusAnalysisBuilder.
VisibilityMaxRadius
¶ Returns or sets the toggle max radius show
-------------------------------------
Getter Method
Signature
VisibilityMaxRadius()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibilityMaxRadius(visibilityMaxRadius)
Parameters: visibilityMaxRadius (bool) – New in version NX8.5.0.
License requirements: None.
VisibilityMinMaxRadiusTangent¶
-
LocalRadiusAnalysisBuilder.
VisibilityMinMaxRadiusTangent
¶ Returns or sets the toggle min radius tangent
-------------------------------------
Getter Method
Signature
VisibilityMinMaxRadiusTangent()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibilityMinMaxRadiusTangent(visibilityMinMaxRadiusTangent)
Parameters: visibilityMinMaxRadiusTangent (bool) – New in version NX8.5.0.
License requirements: None.
VisibilityMinRadius¶
-
LocalRadiusAnalysisBuilder.
VisibilityMinRadius
¶ Returns or sets the toggle min radius show
-------------------------------------
Getter Method
Signature
VisibilityMinRadius()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibilityMinRadius(visibilityMinRadius)
Parameters: visibilityMinRadius (bool) – New in version NX8.5.0.
License requirements: None.
VisibilityRadius¶
-
LocalRadiusAnalysisBuilder.
VisibilityRadius
¶ Returns or sets the toggle radius show
-------------------------------------
Getter Method
Signature
VisibilityRadius()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibilityRadius(visibilityRadius)
Parameters: visibilityRadius (bool) – New in version NX8.5.0.
License requirements: None.
VisibilityURadius¶
-
LocalRadiusAnalysisBuilder.
VisibilityURadius
¶ Returns or sets the toggle uradius show
-------------------------------------
Getter Method
Signature
VisibilityURadius()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibilityURadius(visibilityURadius)
Parameters: visibilityURadius (bool) – New in version NX8.5.0.
License requirements: None.
VisibilityUV¶
-
LocalRadiusAnalysisBuilder.
VisibilityUV
¶ Returns or sets the toggle uv
-------------------------------------
Getter Method
Signature
VisibilityUV()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibilityUV(visibilityUV)
Parameters: visibilityUV (bool) – New in version NX8.5.0.
License requirements: None.
VisibilityUVTangent¶
-
LocalRadiusAnalysisBuilder.
VisibilityUVTangent
¶ Returns or sets the toggle max radius tangent
-------------------------------------
Getter Method
Signature
VisibilityUVTangent()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibilityUVTangent(visibilityUVTangent)
Parameters: visibilityUVTangent (bool) – New in version NX8.5.0.
License requirements: None.
VisibilityVRadius¶
-
LocalRadiusAnalysisBuilder.
VisibilityVRadius
¶ Returns or sets the toggle vradius show
-------------------------------------
Getter Method
Signature
VisibilityVRadius()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibilityVRadius(visibilityVRadius)
Parameters: visibilityVRadius (bool) – New in version NX8.5.0.
License requirements: None.
Method Detail¶
ButtonOpenInformationWindow¶
-
LocalRadiusAnalysisBuilder.
ButtonOpenInformationWindow
¶ TODO: fill in a description for this
Signature
ButtonOpenInformationWindow()
New in version NX8.5.0.
License requirements: None.
Validate¶
-
LocalRadiusAnalysisBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.