HighlightLinesAnalysisBuilderTypes Enumeration¶
NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilder.Types is an alias for NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilderTypes
-
class
NXOpen.GeometricAnalysis.
HighlightLinesAnalysisBuilderTypes
¶ Bases:
object
three types of light methods
Deprecated since version NX8.0.0: Use
NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilder.LightPlacements`
instead.Enum Members
pass through two given surface points. More highlight lines are created between these two highlight lines when light number is more than two. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-