HighlightLinesAnalysisBuilderDisplayMethods Enumeration¶
NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilder.DisplayMethods is an alias for NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilderDisplayMethods
-
class
NXOpen.GeometricAnalysis.
HighlightLinesAnalysisBuilderDisplayMethods
¶ Bases:
object
display methods
Deprecated since version NX8.0.0: Use
NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilder.Types2`
instead.Enum Members
Enum Member Enum Member Description Reflection Create reflection linesProjection Create projection lines-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-