GapFlushnessBuilder Class¶
-
class
NXOpen.GeometricAnalysis.
GapFlushnessBuilder
¶ Bases:
NXOpen.Builder
GapFlushnessBuilder class
To create a new instance of this class, use
NXOpen.GeometricAnalysis.AnalysisObjectCollection.CreateGapFlushnessBuilder
Default values.
Property Value SampleNumber 10 New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BasePanelFaces | Returns the Base Panel face selection |
BasePanelInnerContactCurves | Returns the Base Panel inner contact section |
BasePanelOuterContactCurves | Returns the Base Panel outer contact section |
BasePanelType | Returns or sets the Base Panel type |
CrossSectionCurveOption | Returns or sets the cross section curve option |
CrossSectionCurves | Returns the Cross Section Curves |
EvaluationMode | Returns or sets the evaluation Method |
EvaluationPoint | Returns or sets the evaluation point |
EvaluationType | Returns or sets the evaluation type |
IsNegativeToleranceLabelDisplayed | Returns or sets the Label Display negative tolerance |
IsNominalLabelDisplayed | Returns or sets the Label Display Nominal |
IsPositiveToleranceLabelDisplayed | Returns or sets the Label Display positive tolerance |
LabelDisplayOption | Returns or sets the display option type |
NegativeFlushnessTolerance | Returns or sets the negative tolerance for flushness |
NegativeGapTolerance | Returns or sets the negative tolerance for gap |
NominalFlushness | Returns or sets the nominal value for flushness |
NominalGap | Returns or sets the nominal value for gap |
PositiveFlushnessTolerance | Returns or sets the positive tolerance for flushness |
PositiveGapTolerance | Returns or sets the positive tolerance for gap |
PreviewOption | Returns or sets the preview option |
SampleDistance | Returns the Sample Distance |
SampleNumber | Returns or sets the sample number |
SecondPanelFaces | Returns the Second Panel face selection |
SecondPanelInnerContactCurves | Returns the Second Panel inner contact section |
SecondPanelOuterContactCurves | Returns the Second Panel outer contact section |
SecondPanelType | Returns or sets the Second Panel type |
SectionAlignment | Returns or sets the Section Alignment |
SectionAlignmentDirection | Returns or sets the section alignment vector |
ShowOutRangeLabels | Returns or sets the show out of range labels |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GapFlushnessBuilderDisplayOptions Enumeration | This enum represents Label Display Option type |
GapFlushnessBuilderEvaluationModes Enumeration | This enum represents evaluation mode |
GapFlushnessBuilderEvaluationTypes Enumeration | This enum represents the Gap and Flushness Analysis Object evaluation types |
GapFlushnessBuilderPanelTypes Enumeration | This enum represents panel type |
GapFlushnessBuilderSectionAlignments Enumeration | This enum represents cross-section alignment type |
GapFlushnessBuilderSectionCurveOptions Enumeration | This enum represents Cross Section Curves Options |
Property Detail¶
BasePanelFaces¶
-
GapFlushnessBuilder.
BasePanelFaces
¶ Returns the Base Panel face selection
-------------------------------------
Getter Method
Signature
BasePanelFaces()
Returns: Face collector Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
BasePanelInnerContactCurves¶
-
GapFlushnessBuilder.
BasePanelInnerContactCurves
¶ Returns the Base Panel inner contact section
-------------------------------------
Getter Method
Signature
BasePanelInnerContactCurves()
Returns: curve/edge collector Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
BasePanelOuterContactCurves¶
-
GapFlushnessBuilder.
BasePanelOuterContactCurves
¶ Returns the Base Panel outer contact section
-------------------------------------
Getter Method
Signature
BasePanelOuterContactCurves()
Returns: curve/edge collector Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
BasePanelType¶
-
GapFlushnessBuilder.
BasePanelType
¶ Returns or sets the Base Panel type
-------------------------------------
Getter Method
Signature
BasePanelType()
Returns: Return type: NXOpen.GeometricAnalysis.GapFlushnessBuilderPanelTypes
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
BasePanelType(panelType)
Parameters: panelType ( NXOpen.GeometricAnalysis.GapFlushnessBuilderPanelTypes
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CrossSectionCurveOption¶
-
GapFlushnessBuilder.
CrossSectionCurveOption
¶ Returns or sets the cross section curve option
-------------------------------------
Getter Method
Signature
CrossSectionCurveOption()
Returns: Return type: NXOpen.GeometricAnalysis.GapFlushnessBuilderSectionCurveOptions
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
CrossSectionCurveOption(sectionCurveOption)
Parameters: sectionCurveOption ( NXOpen.GeometricAnalysis.GapFlushnessBuilderSectionCurveOptions
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CrossSectionCurves¶
-
GapFlushnessBuilder.
CrossSectionCurves
¶ Returns the Cross Section Curves
-------------------------------------
Getter Method
Signature
CrossSectionCurves()
Returns: curve/edge collector Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
EvaluationMode¶
-
GapFlushnessBuilder.
EvaluationMode
¶ Returns or sets the evaluation Method
-------------------------------------
Getter Method
Signature
EvaluationMode()
Returns: Return type: NXOpen.GeometricAnalysis.GapFlushnessBuilderEvaluationModes
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
EvaluationMode(evaluationMode)
Parameters: evaluationMode ( NXOpen.GeometricAnalysis.GapFlushnessBuilderEvaluationModes
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
EvaluationPoint¶
-
GapFlushnessBuilder.
EvaluationPoint
¶ Returns or sets the evaluation point
-------------------------------------
Getter Method
Signature
EvaluationPoint()
Returns: Evaluation point Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
EvaluationPoint(evaluationPoint)
Parameters: evaluationPoint ( NXOpen.Point
) – Evaluation pointNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
EvaluationType¶
-
GapFlushnessBuilder.
EvaluationType
¶ Returns or sets the evaluation type
-------------------------------------
Getter Method
Signature
EvaluationType()
Returns: Return type: NXOpen.GeometricAnalysis.GapFlushnessBuilderEvaluationTypes
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
EvaluationType(evaluationType)
Parameters: evaluationType ( NXOpen.GeometricAnalysis.GapFlushnessBuilderEvaluationTypes
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsNegativeToleranceLabelDisplayed¶
-
GapFlushnessBuilder.
IsNegativeToleranceLabelDisplayed
¶ Returns or sets the Label Display negative tolerance
-------------------------------------
Getter Method
Signature
IsNegativeToleranceLabelDisplayed()
Returns: Return type: bool New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
IsNegativeToleranceLabelDisplayed(showlabelNegative)
Parameters: showlabelNegative (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsNominalLabelDisplayed¶
-
GapFlushnessBuilder.
IsNominalLabelDisplayed
¶ Returns or sets the Label Display Nominal
-------------------------------------
Getter Method
Signature
IsNominalLabelDisplayed()
Returns: Return type: bool New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
IsNominalLabelDisplayed(showlabelNominal)
Parameters: showlabelNominal (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsPositiveToleranceLabelDisplayed¶
-
GapFlushnessBuilder.
IsPositiveToleranceLabelDisplayed
¶ Returns or sets the Label Display positive tolerance
-------------------------------------
Getter Method
Signature
IsPositiveToleranceLabelDisplayed()
Returns: Return type: bool New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
IsPositiveToleranceLabelDisplayed(showlabelPositive)
Parameters: showlabelPositive (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
LabelDisplayOption¶
-
GapFlushnessBuilder.
LabelDisplayOption
¶ Returns or sets the display option type
-------------------------------------
Getter Method
Signature
LabelDisplayOption()
Returns: Return type: NXOpen.GeometricAnalysis.GapFlushnessBuilderDisplayOptions
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
LabelDisplayOption(displayOption)
Parameters: displayOption ( NXOpen.GeometricAnalysis.GapFlushnessBuilderDisplayOptions
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
NegativeFlushnessTolerance¶
-
GapFlushnessBuilder.
NegativeFlushnessTolerance
¶ Returns or sets the negative tolerance for flushness
-------------------------------------
Getter Method
Signature
NegativeFlushnessTolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
NegativeFlushnessTolerance(negativeTolFlush)
Parameters: negativeTolFlush (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
NegativeGapTolerance¶
-
GapFlushnessBuilder.
NegativeGapTolerance
¶ Returns or sets the negative tolerance for gap
-------------------------------------
Getter Method
Signature
NegativeGapTolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
NegativeGapTolerance(negativeTolGap)
Parameters: negativeTolGap (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
NominalFlushness¶
-
GapFlushnessBuilder.
NominalFlushness
¶ Returns or sets the nominal value for flushness
-------------------------------------
Getter Method
Signature
NominalFlushness()
Returns: Return type: float New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
NominalFlushness(nominalFlush)
Parameters: nominalFlush (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
NominalGap¶
-
GapFlushnessBuilder.
NominalGap
¶ Returns or sets the nominal value for gap
-------------------------------------
Getter Method
Signature
NominalGap()
Returns: Return type: float New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
NominalGap(nominalGap)
Parameters: nominalGap (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
PositiveFlushnessTolerance¶
-
GapFlushnessBuilder.
PositiveFlushnessTolerance
¶ Returns or sets the positive tolerance for flushness
-------------------------------------
Getter Method
Signature
PositiveFlushnessTolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
PositiveFlushnessTolerance(positiveTolFlush)
Parameters: positiveTolFlush (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
PositiveGapTolerance¶
-
GapFlushnessBuilder.
PositiveGapTolerance
¶ Returns or sets the positive tolerance for gap
-------------------------------------
Getter Method
Signature
PositiveGapTolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
PositiveGapTolerance(positiveTolGap)
Parameters: positiveTolGap (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
PreviewOption¶
-
GapFlushnessBuilder.
PreviewOption
¶ Returns or sets the preview option
-------------------------------------
Getter Method
Signature
PreviewOption()
Returns: Return type: bool New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
PreviewOption(previewOption)
Parameters: previewOption (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SampleDistance¶
-
GapFlushnessBuilder.
SampleDistance
¶ Returns the Sample Distance
-------------------------------------
Getter Method
Signature
SampleDistance()
Returns: Sample distance Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SampleNumber¶
-
GapFlushnessBuilder.
SampleNumber
¶ Returns or sets the sample number
-------------------------------------
Getter Method
Signature
SampleNumber()
Returns: Return type: int New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
SampleNumber(sampleNumber)
Parameters: sampleNumber (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SecondPanelFaces¶
-
GapFlushnessBuilder.
SecondPanelFaces
¶ Returns the Second Panel face selection
-------------------------------------
Getter Method
Signature
SecondPanelFaces()
Returns: Face collector Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SecondPanelInnerContactCurves¶
-
GapFlushnessBuilder.
SecondPanelInnerContactCurves
¶ Returns the Second Panel inner contact section
-------------------------------------
Getter Method
Signature
SecondPanelInnerContactCurves()
Returns: curve/edge collector Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SecondPanelOuterContactCurves¶
-
GapFlushnessBuilder.
SecondPanelOuterContactCurves
¶ Returns the Second Panel outer contact section
-------------------------------------
Getter Method
Signature
SecondPanelOuterContactCurves()
Returns: curve/edge collector Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SecondPanelType¶
-
GapFlushnessBuilder.
SecondPanelType
¶ Returns or sets the Second Panel type
-------------------------------------
Getter Method
Signature
SecondPanelType()
Returns: Return type: NXOpen.GeometricAnalysis.GapFlushnessBuilderPanelTypes
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
SecondPanelType(panelType)
Parameters: panelType ( NXOpen.GeometricAnalysis.GapFlushnessBuilderPanelTypes
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SectionAlignment¶
-
GapFlushnessBuilder.
SectionAlignment
¶ Returns or sets the Section Alignment
-------------------------------------
Getter Method
Signature
SectionAlignment()
Returns: Return type: NXOpen.GeometricAnalysis.GapFlushnessBuilderSectionAlignments
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
SectionAlignment(sectionAlignment)
Parameters: sectionAlignment ( NXOpen.GeometricAnalysis.GapFlushnessBuilderSectionAlignments
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SectionAlignmentDirection¶
-
GapFlushnessBuilder.
SectionAlignmentDirection
¶ Returns or sets the section alignment vector
-------------------------------------
Getter Method
Signature
SectionAlignmentDirection()
Returns: Section Alignment Direction vector Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
SectionAlignmentDirection(sectionAlignmentDirection)
Parameters: sectionAlignmentDirection ( NXOpen.Direction
) – Section Alignment Direction vectorNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ShowOutRangeLabels¶
-
GapFlushnessBuilder.
ShowOutRangeLabels
¶ Returns or sets the show out of range labels
-------------------------------------
Getter Method
Signature
ShowOutRangeLabels()
Returns: Return type: bool New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
ShowOutRangeLabels(showOutRangeLabels)
Parameters: showOutRangeLabels (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
GapFlushnessBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.