DeviationChecking Class¶
-
class
NXOpen.GeometricAnalysis.
DeviationChecking
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.GeometricAnalysis.DeviationChecking
To create a new instance of this class, use
NXOpen.GeometricAnalysis.AnalysisManager.CreateDeviationCheckingObject
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance to be used for the deviation checking |
Curve | Returns the curve - required for the deviation checking when NXOpen.GeometricAnalysis.DeviationChecking.Type` is set to NXOpen.GeometricAnalysis.DeviationCheckingTypes.CurveToFace . |
DeviationOption | Returns or sets the number or type of deviations to be shown for the deviation checking |
DistanceTolerance | Returns or sets the distance tolerance to be used for the deviation checking |
FaceOfFirstEdge | Returns the face associated with the first edge or edge - required for the deviation checking when NXOpen.GeometricAnalysis.DeviationChecking.Type` is set to NXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToEdge or NXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToFace . |
FaceOfSecondEdge | Returns the face associated with the second edge - required for the deviation checking when NXOpen.GeometricAnalysis.DeviationChecking.Type` is set to NXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToEdge . |
FirstCurve | Returns the first curve or edge - required for the deviation checking when NXOpen.GeometricAnalysis.DeviationChecking.Type` is set to NXOpen.GeometricAnalysis.DeviationCheckingTypes.CurveToCurve . |
FirstEdge | Returns the first edge or edge - required for the deviation checking when NXOpen.GeometricAnalysis.DeviationChecking.Type` is set to NXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToEdge or NXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToFace . |
FirstFace | Returns the first face - required for the deviation checking when NXOpen.GeometricAnalysis.DeviationChecking.Type` is set to NXOpen.GeometricAnalysis.DeviationCheckingTypes.FaceToFace . |
NumberCheckPoints | Returns or sets the number of check points to be shown for the deviation checking - required when NXOpen.GeometricAnalysis.DeviationChecking.Type` is set to NXOpen.GeometricAnalysis.DeviationCheckingTypes.CurveToCurve or NXOpen.GeometricAnalysis.DeviationCheckingTypes.CurveToFace or NXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToFace or NXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToEdge . |
NumberUcheckPoints | Returns or sets the number of u check points to be shown for the deviation checking - required when NXOpen.GeometricAnalysis.DeviationChecking.Type` is set to NXOpen.GeometricAnalysis.DeviationCheckingTypes.FaceToFace |
NumberVcheckPoints | Returns or sets the number of v check points to be shown for the deviation checking - required when NXOpen.GeometricAnalysis.DeviationChecking.Type` is set to NXOpen.GeometricAnalysis.DeviationCheckingTypes.FaceToFace |
SecondCurve | Returns the second curve or edge - required for the deviation checking when NXOpen.GeometricAnalysis.DeviationChecking.Type` is set to NXOpen.GeometricAnalysis.DeviationCheckingTypes.CurveToCurve . |
SecondEdge | Returns the second edge - required for the deviation checking when NXOpen.GeometricAnalysis.DeviationChecking.Type` is set to NXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToEdge . |
SecondFace | Returns the second face - required for the deviation checking when NXOpen.GeometricAnalysis.DeviationChecking.Type` is set to NXOpen.GeometricAnalysis.DeviationCheckingTypes.FaceToFace or the face - required for the deviation checking when NXOpen.GeometricAnalysis.DeviationChecking.Type` is set to NXOpen.GeometricAnalysis.DeviationCheckingTypes.CurveToFace or NXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToFace . |
Tag | Returns the Tag for this object. |
Type | Returns or sets the deviation checking type. |
Methods¶
Method | Description |
---|---|
Check | Performs deviation checking. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DeviationCheckingDeviationOptions Enumeration | the deviation type to be shown |
DeviationCheckingTypes Enumeration | the type of deviation checking to be performed |
Property Detail¶
AngleTolerance¶
-
DeviationChecking.
AngleTolerance
¶ Returns or sets the angle tolerance to be used for the deviation checking
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance(angleTolerance)
Parameters: angleTolerance (float) – New in version NX6.0.0.
License requirements: None.
Curve¶
-
DeviationChecking.
Curve
¶ Returns the curve - required for the deviation checking when
NXOpen.GeometricAnalysis.DeviationChecking.Type`
is set toNXOpen.GeometricAnalysis.DeviationCheckingTypes.CurveToFace
.-------------------------------------
Getter Method
Signature
Curve()
Returns: Return type: NXOpen.SelectIBaseCurve
New in version NX6.0.0.
License requirements: None.
DeviationOption¶
-
DeviationChecking.
DeviationOption
¶ Returns or sets the number or type of deviations to be shown for the deviation checking
-------------------------------------
Getter Method
Signature
DeviationOption()
Returns: Return type: NXOpen.GeometricAnalysis.DeviationCheckingDeviationOptions
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeviationOption(deviationOption)
Parameters: deviationOption ( NXOpen.GeometricAnalysis.DeviationCheckingDeviationOptions
) –New in version NX6.0.0.
License requirements: None.
DistanceTolerance¶
-
DeviationChecking.
DistanceTolerance
¶ Returns or sets the distance tolerance to be used for the deviation checking
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX6.0.0.
License requirements: None.
FaceOfFirstEdge¶
-
DeviationChecking.
FaceOfFirstEdge
¶ Returns the face associated with the first edge or edge - required for the deviation checking when
NXOpen.GeometricAnalysis.DeviationChecking.Type`
is set toNXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToEdge
orNXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToFace
.-------------------------------------
Getter Method
Signature
FaceOfFirstEdge()
Returns: Return type: NXOpen.SelectIParameterizedSurface
New in version NX6.0.0.
License requirements: None.
FaceOfSecondEdge¶
-
DeviationChecking.
FaceOfSecondEdge
¶ Returns the face associated with the second edge - required for the deviation checking when
NXOpen.GeometricAnalysis.DeviationChecking.Type`
is set toNXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToEdge
.-------------------------------------
Getter Method
Signature
FaceOfSecondEdge()
Returns: Return type: NXOpen.SelectIParameterizedSurface
New in version NX6.0.0.
License requirements: None.
FirstCurve¶
-
DeviationChecking.
FirstCurve
¶ Returns the first curve or edge - required for the deviation checking when
NXOpen.GeometricAnalysis.DeviationChecking.Type`
is set toNXOpen.GeometricAnalysis.DeviationCheckingTypes.CurveToCurve
.-------------------------------------
Getter Method
Signature
FirstCurve()
Returns: Return type: NXOpen.SelectIBaseCurve
New in version NX6.0.0.
License requirements: None.
FirstEdge¶
-
DeviationChecking.
FirstEdge
¶ Returns the first edge or edge - required for the deviation checking when
NXOpen.GeometricAnalysis.DeviationChecking.Type`
is set toNXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToEdge
orNXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToFace
.-------------------------------------
Getter Method
Signature
FirstEdge()
Returns: Return type: NXOpen.SelectIBaseCurve
New in version NX6.0.0.
License requirements: None.
FirstFace¶
-
DeviationChecking.
FirstFace
¶ Returns the first face - required for the deviation checking when
NXOpen.GeometricAnalysis.DeviationChecking.Type`
is set toNXOpen.GeometricAnalysis.DeviationCheckingTypes.FaceToFace
.-------------------------------------
Getter Method
Signature
FirstFace()
Returns: Return type: NXOpen.SelectIParameterizedSurface
New in version NX6.0.0.
License requirements: None.
NumberCheckPoints¶
-
DeviationChecking.
NumberCheckPoints
¶ Returns or sets the number of check points to be shown for the deviation checking - required when
NXOpen.GeometricAnalysis.DeviationChecking.Type`
is set toNXOpen.GeometricAnalysis.DeviationCheckingTypes.CurveToCurve
orNXOpen.GeometricAnalysis.DeviationCheckingTypes.CurveToFace
orNXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToFace
orNXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToEdge
.-------------------------------------
Getter Method
Signature
NumberCheckPoints()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberCheckPoints(numberCheckPoints)
Parameters: numberCheckPoints (int) – New in version NX6.0.0.
License requirements: None.
NumberUcheckPoints¶
-
DeviationChecking.
NumberUcheckPoints
¶ Returns or sets the number of u check points to be shown for the deviation checking - required when
NXOpen.GeometricAnalysis.DeviationChecking.Type`
is set toNXOpen.GeometricAnalysis.DeviationCheckingTypes.FaceToFace
-------------------------------------
Getter Method
Signature
NumberUcheckPoints()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberUcheckPoints(numberUCheckPoints)
Parameters: numberUCheckPoints (int) – New in version NX6.0.0.
License requirements: None.
NumberVcheckPoints¶
-
DeviationChecking.
NumberVcheckPoints
¶ Returns or sets the number of v check points to be shown for the deviation checking - required when
NXOpen.GeometricAnalysis.DeviationChecking.Type`
is set toNXOpen.GeometricAnalysis.DeviationCheckingTypes.FaceToFace
-------------------------------------
Getter Method
Signature
NumberVcheckPoints()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberVcheckPoints(numberVCheckPoints)
Parameters: numberVCheckPoints (int) – New in version NX6.0.0.
License requirements: None.
SecondCurve¶
-
DeviationChecking.
SecondCurve
¶ Returns the second curve or edge - required for the deviation checking when
NXOpen.GeometricAnalysis.DeviationChecking.Type`
is set toNXOpen.GeometricAnalysis.DeviationCheckingTypes.CurveToCurve
.-------------------------------------
Getter Method
Signature
SecondCurve()
Returns: Return type: NXOpen.SelectIBaseCurve
New in version NX6.0.0.
License requirements: None.
SecondEdge¶
-
DeviationChecking.
SecondEdge
¶ Returns the second edge - required for the deviation checking when
NXOpen.GeometricAnalysis.DeviationChecking.Type`
is set toNXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToEdge
.-------------------------------------
Getter Method
Signature
SecondEdge()
Returns: Return type: NXOpen.SelectIBaseCurve
New in version NX6.0.0.
License requirements: None.
SecondFace¶
-
DeviationChecking.
SecondFace
¶ Returns the second face - required for the deviation checking when
NXOpen.GeometricAnalysis.DeviationChecking.Type`
is set toNXOpen.GeometricAnalysis.DeviationCheckingTypes.FaceToFace
or the face - required for the deviation checking whenNXOpen.GeometricAnalysis.DeviationChecking.Type`
is set toNXOpen.GeometricAnalysis.DeviationCheckingTypes.CurveToFace
orNXOpen.GeometricAnalysis.DeviationCheckingTypes.EdgeToFace
.-------------------------------------
Getter Method
Signature
SecondFace()
Returns: Return type: NXOpen.SelectIParameterizedSurface
New in version NX6.0.0.
License requirements: None.
Type¶
-
DeviationChecking.
Type
¶ Returns or sets the deviation checking type.
Depending on the value of the deviation checking type, different inputs are required. See the documentation for each of the inputs.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.GeometricAnalysis.DeviationCheckingTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.GeometricAnalysis.DeviationCheckingTypes
) –New in version NX6.0.0.
License requirements: None.
Method Detail¶
Check¶
-
DeviationChecking.
Check
¶ Performs deviation checking.
Before calling this method, set property
NXOpen.GeometricAnalysis.DeviationChecking.Type`
to specify the type of deviation checking, and the two objects (curve/face/edge) to be used the deviation checking. The type of the objects required depends onNXOpen.GeometricAnalysis.DeviationChecking.Type`
set above. Also set the number check points to be displayed or u and v check points, the distance tolerance, and the angle tolerance before calling the methodNXOpen.GeometricAnalysis.DeviationChecking.Check
.NXOpen.GeometricAnalysis.DeviationChecking.Check
displays the deviation as per the specification above in the graphics and lists in the information window of NX.Signature
Check()
New in version NX6.0.0.
License requirements: None.
Validate¶
-
DeviationChecking.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.