CurveContinuityBuilder Class¶
-
class
NXOpen.GeometricAnalysis.
CurveContinuityBuilder
¶ Bases:
NXOpen.Builder
Represents a curve continuity builder
To create a new instance of this class, use
NXOpen.GeometricAnalysis.AnalysisObjectCollection.CreateCurveContinuityBuilder
Default values.
Property Value EndPointX 0 EndPointY 0 EndPointZ 0 G0Check 1 G1Check 0 G2Check 0 G3Check 0 ShowNeedle 1 New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
EndPointX | Returns or sets the end point x value |
EndPointY | Returns or sets the end point y value |
EndPointZ | Returns or sets the end point z value |
G0Check | Returns or sets the G0 check |
G1Check | Returns or sets the G1 check |
G2Check | Returns or sets the G2 check |
G3Check | Returns or sets the G3 check |
SelectCurve | Returns the select curve |
SelectObject | Returns the select object |
ShowNeedle | Returns or sets the show needle |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EndPointX¶
-
CurveContinuityBuilder.
EndPointX
¶ Returns or sets the end point x value
-------------------------------------
Getter Method
Signature
EndPointX()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPointX(endPointX)
Parameters: endPointX (float) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
EndPointY¶
-
CurveContinuityBuilder.
EndPointY
¶ Returns or sets the end point y value
-------------------------------------
Getter Method
Signature
EndPointY()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPointY(endPointY)
Parameters: endPointY (float) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
EndPointZ¶
-
CurveContinuityBuilder.
EndPointZ
¶ Returns or sets the end point z value
-------------------------------------
Getter Method
Signature
EndPointZ()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPointZ(endPointZ)
Parameters: endPointZ (float) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
G0Check¶
-
CurveContinuityBuilder.
G0Check
¶ Returns or sets the G0 check
-------------------------------------
Getter Method
Signature
G0Check()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G0Check(g0Check)
Parameters: g0Check (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
G1Check¶
-
CurveContinuityBuilder.
G1Check
¶ Returns or sets the G1 check
-------------------------------------
Getter Method
Signature
G1Check()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G1Check(g1Check)
Parameters: g1Check (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
G2Check¶
-
CurveContinuityBuilder.
G2Check
¶ Returns or sets the G2 check
-------------------------------------
Getter Method
Signature
G2Check()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G2Check(g2Check)
Parameters: g2Check (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
G3Check¶
-
CurveContinuityBuilder.
G3Check
¶ Returns or sets the G3 check
-------------------------------------
Getter Method
Signature
G3Check()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G3Check(g3Check)
Parameters: g3Check (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
SelectCurve¶
-
CurveContinuityBuilder.
SelectCurve
¶ Returns the select curve
-------------------------------------
Getter Method
Signature
SelectCurve()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
SelectObject¶
-
CurveContinuityBuilder.
SelectObject
¶ Returns the select object
-------------------------------------
Getter Method
Signature
SelectObject()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
ShowNeedle¶
-
CurveContinuityBuilder.
ShowNeedle
¶ Returns or sets the show needle
-------------------------------------
Getter Method
Signature
ShowNeedle()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowNeedle(showNeedle)
Parameters: showNeedle (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Method Detail¶
Validate¶
-
CurveContinuityBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.