CopyCutBuilder Class¶
-
class
NXOpen.Gateway.
CopyCutBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Gateway.CopyCutBuilder
To create a new instance of this class, use
NXOpen.ClipboardOperationsManager.CreateCopyCutBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
CanCopyAsSketch | Returns or sets a flag indicating whether to copy as sketch curves or not |
DestinationFilename | Returns or sets the string of the filename to which to copy or cut the objects to |
InitialCopyLocation | Returns or sets the initial copy location mainly used to define default copy location of sketch objects |
IsCut | Returns or sets a flag indicating whether it is a copy or cut operation |
Tag | Returns the Tag for this object. |
ToClipboard | Returns or sets a flag indicating whether copy cut to clipboard or copy cut to a file |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCopyCutStatus | Gets the status of copy-cut operation @return |
GetNonExportableObjects | Gets all non-exportable objects @return All the non-exportable objects |
GetObject | Returns the object currently being edited by this builder. |
GetObjects | Gets all objects to be copied or to be cut @return All the objects to be copied or to be cut |
ResetInitialCopyLocation | Reset the initial copy location. |
SetObjects | Sets all objects to be copied or to be cut |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CopyCutBuilderStatus Enumeration | Status of Copy or Cut Operation |
Property Detail¶
CanCopyAsSketch¶
-
CopyCutBuilder.
CanCopyAsSketch
¶ Returns or sets a flag indicating whether to copy as sketch curves or not
-------------------------------------
Getter Method
Signature
CanCopyAsSketch()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanCopyAsSketch(canCopyAsSketch)
Parameters: canCopyAsSketch (bool) – New in version NX7.5.0.
License requirements: None.
DestinationFilename¶
-
CopyCutBuilder.
DestinationFilename
¶ Returns or sets the string of the filename to which to copy or cut the objects to
-------------------------------------
Getter Method
Signature
DestinationFilename()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DestinationFilename(filename)
Parameters: filename (str) – New in version NX7.5.0.
License requirements: None.
InitialCopyLocation¶
-
CopyCutBuilder.
InitialCopyLocation
¶ Returns or sets the initial copy location mainly used to define default copy location of sketch objects
-------------------------------------
Getter Method
Signature
InitialCopyLocation()
Returns: Copy location in absolute coordinates Return type: NXOpen.Point3d
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InitialCopyLocation(copyLocation)
Parameters: copyLocation ( NXOpen.Point3d
) – Copy location in absolute coordinatesNew in version NX7.5.0.
License requirements: None.
IsCut¶
-
CopyCutBuilder.
IsCut
¶ Returns or sets a flag indicating whether it is a copy or cut operation
-------------------------------------
Getter Method
Signature
IsCut()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsCut(isCut)
Parameters: isCut (bool) – New in version NX7.5.0.
License requirements: None.
ToClipboard¶
-
CopyCutBuilder.
ToClipboard
¶ Returns or sets a flag indicating whether copy cut to clipboard or copy cut to a file
-------------------------------------
Getter Method
Signature
ToClipboard()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToClipboard(isToClipboard)
Parameters: isToClipboard (bool) – New in version NX7.5.0.
License requirements: None.
Method Detail¶
GetCopyCutStatus¶
-
CopyCutBuilder.
GetCopyCutStatus
¶ Gets the status of copy-cut operation
Signature
GetCopyCutStatus()
Returns: Return type: NXOpen.Gateway.CopyCutBuilderStatus
New in version NX7.5.0.
License requirements: None.
GetNonExportableObjects¶
-
CopyCutBuilder.
GetNonExportableObjects
¶ Gets all non-exportable objects
Signature
GetNonExportableObjects()
Returns: All the non-exportable objects Return type: list of NXOpen.NXObject
New in version NX7.5.0.
License requirements: None.
GetObjects¶
-
CopyCutBuilder.
GetObjects
¶ Gets all objects to be copied or to be cut
Signature
GetObjects()
Returns: All the objects to be copied or to be cut Return type: list of NXOpen.NXObject
New in version NX7.5.0.
License requirements: None.
ResetInitialCopyLocation¶
-
CopyCutBuilder.
ResetInitialCopyLocation
¶ Reset the initial copy location.
After this previously set initial copy location will not be used
Signature
ResetInitialCopyLocation()
New in version NX7.5.0.
License requirements: None.
SetObjects¶
-
CopyCutBuilder.
SetObjects
¶ Sets all objects to be copied or to be cut
Signature
SetObjects(objects)
Parameters: objects (list of NXOpen.NXObject
) – All the objects to be copied or to be cutNew in version NX7.5.0.
License requirements: None.
Validate¶
-
CopyCutBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.