FileNew Class¶
-
class
NXOpen.
FileNew
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.FileNew
This class is not directly created. The creator of the super class does the real work
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Application | Returns or sets the application type for the new file being created |
ApplicationName | Returns or sets the application type for the new file being created Use NXOpen.FileNew.GetApplicationNames to get valid application names. |
DesignElementState | Returns or sets the state for the new design element. |
DesignElementType | Returns or sets the design element type for the new design element. |
ItemType | Returns or sets the item type for the new file. |
MakeDisplayedPart | Returns or sets the property that controls if the new file should be made the displayed part |
MasterFileName | Returns or sets the name of the master model part to be referenced. |
NewFileName | Returns or sets the name of the new file being created |
RelationType | Returns or sets the relation type of the underlying template which is used for the new file being created. |
Specialization | Returns or sets the specialization for the new file |
Tag | Returns the Tag for this object. |
TemplateFileName | Returns or sets the name of the template part from which to create the new file |
TemplatePresentationName | Returns or sets the presentation name of the underlying template which is used for the new file being created |
TemplateType | Returns or sets the template type for the new file being created |
Units | Returns or sets the units for the new file being created |
UseBlankTemplate | Returns or sets the property that controls if the new file should be created using a blank template. |
UsesMasterModel | Returns or sets the uses master model flag of the underlying template which is used for the new file being created. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAddMasterFlag | Returns logical value to indicate whether master to be added as child component @return whether master to be added as child component |
GetApplicationNames | Returns all registered application names. |
GetAvailableTemplates | Returns the available templates for the session @return array of available template names |
GetCanCreateAltrep | Gets the flag specifying if the current template customization allows Alternate representation creation using the template @return |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAddMasterFlag | Sets addMaster flag |
SetCanCreateAltrep | Sets the flag specifying if the current template customization allows Alternate representation creation using the template |
SetPartOperationCreateBuilder | Sets NXOpen.PDM.PartOperationBuilder |
SetProjectsData | Teamcenter projects data |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Application¶
-
FileNew.
Application
¶ Returns or sets the application type for the new file being created
-------------------------------------
Getter Method
Signature
Application()
Returns: Return type: NXOpen.FileNewApplication
New in version NX5.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.FileNew.ApplicationName
that takes a string name instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Application(application)
Parameters: application ( NXOpen.FileNewApplication
) –New in version NX5.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.FileNew.ApplicationName
that takes a string name instead.License requirements: None.
ApplicationName¶
-
FileNew.
ApplicationName
¶ Returns or sets the application type for the new file being created Use
NXOpen.FileNew.GetApplicationNames
to get valid application names.-------------------------------------
Getter Method
Signature
ApplicationName()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApplicationName(application)
Parameters: application (str) – New in version NX5.0.0.
License requirements: None.
DesignElementState¶
-
FileNew.
DesignElementState
¶ Returns or sets the state for the new design element.
It can be a comma separated string in case the underlying template supports multiple design element states
-------------------------------------
Getter Method
Signature
DesignElementState()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DesignElementState(deState)
Parameters: deState (str) – New in version NX8.5.0.
License requirements: None.
DesignElementType¶
-
FileNew.
DesignElementType
¶ Returns or sets the design element type for the new design element.
It can be a comma separated string in case the underlying template supports multiple design element types
-------------------------------------
Getter Method
Signature
DesignElementType()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DesignElementType(deType)
Parameters: deType (str) – New in version NX8.5.0.
License requirements: None.
ItemType¶
-
FileNew.
ItemType
¶ Returns or sets the item type for the new file.
It can be a comma separated string in case the underlying template supports multiple item types
-------------------------------------
Getter Method
Signature
ItemType()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ItemType(itemType)
Parameters: itemType (str) – New in version NX8.5.0.
License requirements: None.
MakeDisplayedPart¶
-
FileNew.
MakeDisplayedPart
¶ Returns or sets the property that controls if the new file should be made the displayed part
-------------------------------------
Getter Method
Signature
MakeDisplayedPart()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MakeDisplayedPart(makeDisplayedPart)
Parameters: makeDisplayedPart (bool) – New in version NX5.0.0.
License requirements: None.
MasterFileName¶
-
FileNew.
MasterFileName
¶ Returns or sets the name of the master model part to be referenced.
May be NULL if creating a master part
-------------------------------------
Getter Method
Signature
MasterFileName()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MasterFileName(masterFileName)
Parameters: masterFileName (str) – New in version NX5.0.0.
License requirements: None.
NewFileName¶
-
FileNew.
NewFileName
¶ Returns or sets the name of the new file being created
-------------------------------------
Getter Method
Signature
NewFileName()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewFileName(fileName)
Parameters: fileName (str) – New in version NX5.0.0.
License requirements: None.
RelationType¶
-
FileNew.
RelationType
¶ Returns or sets the relation type of the underlying template which is used for the new file being created.
If set to ‘Specification’, this means non-master template is used for part creation and it will require
NXOpen.FileNew.UsesMasterModel
to be set to ‘Yes’-------------------------------------
Getter Method
Signature
RelationType()
Returns: Return type: str New in version NX8.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
RelationType(relationType)
Parameters: relationType (str) – New in version NX8.5.3.
License requirements: None.
Specialization¶
-
FileNew.
Specialization
¶ Returns or sets the specialization for the new file
-------------------------------------
Getter Method
Signature
Specialization()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Specialization(specialization)
Parameters: specialization (str) – New in version NX8.5.0.
License requirements: None.
TemplateFileName¶
-
FileNew.
TemplateFileName
¶ Returns or sets the name of the template part from which to create the new file
-------------------------------------
Getter Method
Signature
TemplateFileName()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TemplateFileName(templateFileName)
Parameters: templateFileName (str) – New in version NX5.0.0.
License requirements: None.
TemplatePresentationName¶
-
FileNew.
TemplatePresentationName
¶ Returns or sets the presentation name of the underlying template which is used for the new file being created
-------------------------------------
Getter Method
Signature
TemplatePresentationName()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TemplatePresentationName(presentationName)
Parameters: presentationName (str) – New in version NX8.5.0.
License requirements: None.
TemplateType¶
-
FileNew.
TemplateType
¶ Returns or sets the template type for the new file being created
-------------------------------------
Getter Method
Signature
TemplateType()
Returns: Return type: NXOpen.FileNewTemplateType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TemplateType(templateType)
Parameters: templateType ( NXOpen.FileNewTemplateType
) –New in version NX8.0.0.
License requirements: None.
Units¶
-
FileNew.
Units
¶ Returns or sets the units for the new file being created
-------------------------------------
Getter Method
Signature
Units()
Returns: Return type: NXOpen.PartUnits
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Units(units)
Parameters: units ( NXOpen.PartUnits
) –New in version NX5.0.0.
License requirements: None.
UseBlankTemplate¶
-
FileNew.
UseBlankTemplate
¶ Returns or sets the property that controls if the new file should be created using a blank template.
If set to False, then a valid file name for an existing template part file must be supplied to
NXOpen.FileNew.TemplateFileName
. If set to True, this means that no template is used during creation.Note: This property should be set to True only while creating traditional items with template type set as
FileNewTemplateType.Item
-------------------------------------
Getter Method
Signature
UseBlankTemplate()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseBlankTemplate(useBlankTemplate)
Parameters: useBlankTemplate (bool) – New in version NX5.0.0.
License requirements: None.
UsesMasterModel¶
-
FileNew.
UsesMasterModel
¶ Returns or sets the uses master model flag of the underlying template which is used for the new file being created.
If set to ‘No’, this means that master template is used for part creation. If set to ‘Yes’, this means non-master template is used and it will require master model part to be specified for part creation
-------------------------------------
Getter Method
Signature
UsesMasterModel()
Returns: Return type: str New in version NX8.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
UsesMasterModel(usesMasterModel)
Parameters: usesMasterModel (str) – New in version NX8.5.3.
License requirements: None.
Method Detail¶
GetAddMasterFlag¶
-
FileNew.
GetAddMasterFlag
¶ Returns logical value to indicate whether master to be added as child component
Signature
GetAddMasterFlag()
Returns: whether master to be added as child component Return type: bool New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.PDM.PartOperationCreateBuilder.GetAddMaster
to get addMaster flag.License requirements: None.
GetApplicationNames¶
-
FileNew.
GetApplicationNames
¶ Returns all registered application names.
These name should be used while setting the application name in
ApplicationName
.Signature
GetApplicationNames()
Returns: All registered application names Return type: list of str New in version NX9.0.0.
License requirements: None.
GetAvailableTemplates¶
-
FileNew.
GetAvailableTemplates
¶ Returns the available templates for the session
Signature
GetAvailableTemplates()
Returns: array of available template names Return type: list of str New in version NX6.0.0.
License requirements: None.
GetCanCreateAltrep¶
-
FileNew.
GetCanCreateAltrep
¶ Gets the flag specifying if the current template customization allows Alternate representation creation using the template
Signature
GetCanCreateAltrep()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
SetAddMasterFlag¶
-
FileNew.
SetAddMasterFlag
¶ Sets addMaster flag
Signature
SetAddMasterFlag(addMaster)
Parameters: addMaster (bool) – whether master to be added as child component New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.PDM.PartOperationCreateBuilder.SetAddMaster
to set addMaster flag.License requirements: None.
SetCanCreateAltrep¶
-
FileNew.
SetCanCreateAltrep
¶ Sets the flag specifying if the current template customization allows Alternate representation creation using the template
Signature
SetCanCreateAltrep(createAltrep)
Parameters: createAltrep (bool) – New in version NX10.0.0.
License requirements: None.
SetPartOperationCreateBuilder¶
-
FileNew.
SetPartOperationCreateBuilder
¶ Sets
NXOpen.PDM.PartOperationBuilder
Signature
SetPartOperationCreateBuilder(partOperationBuilder)
Parameters: partOperationBuilder ( NXOpen.PDM.PartOperationBuilder
) –New in version NX10.0.0.
License requirements: None.
SetProjectsData¶
-
FileNew.
SetProjectsData
¶ Teamcenter projects data
Signature
SetProjectsData(projectName, assignmentState)
Parameters: - projectName (list of str) – name of the project NOTE: The full Unicode character set is not supported for this parameter.
- assignmentState (list of int) – assignment state
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Session.AssignRemoveProjects
to assign/remove projects.License requirements: None.
Validate¶
-
FileNew.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.