WheelFixingBuilderWheelSizeType Enumeration¶
NXOpen.Features.VehicleDesign.WheelFixingBuilder.WheelSizeType is an alias for NXOpen.Features.VehicleDesign.WheelFixingBuilderWheelSizeType
-
class
NXOpen.Features.VehicleDesign.
WheelFixingBuilderWheelSizeType
¶ Bases:
object
Represents the wheel size used to indicate if the wheel fixing is based on static radius or the diameter of the wheels.
Enum Members
Enum Member Enum Member Description StaticRadius Diameter -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-