WheelCoveringBuilderRequirementsControlType Enumeration¶
NXOpen.Features.VehicleDesign.WheelCoveringBuilder.RequirementsControlType is an alias for NXOpen.Features.VehicleDesign.WheelCoveringBuilderRequirementsControlType
-
class
NXOpen.Features.VehicleDesign.
WheelCoveringBuilderRequirementsControlType
¶ Bases:
object
Represents the requirements control types to define the wheel covering.
Enum Members
Enum Member Enum Member Description StandardDriven Represents the option for reading parameters from the config fileUserDefined Represents the option for input of user defined parameters-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-