TireEnvelopeBuilderSuspensionTemplateType Enumeration¶
NXOpen.Features.VehicleDesign.TireEnvelopeBuilder.SuspensionTemplateType is an alias for NXOpen.Features.VehicleDesign.TireEnvelopeBuilderSuspensionTemplateType
-
class
NXOpen.Features.VehicleDesign.
TireEnvelopeBuilderSuspensionTemplateType
¶ Bases:
object
Settings to indicate the defined suspension template to use.
Enum Members
Enum Member Enum Member Description MacPhersonStrut Use the MacPherson Strut suspension template.ShortLongArmwithSteering Use the Short-Long Arm with steering suspension template.ShortLongArmwithoutSteering Use the Short-Long Arm without steering suspension template.FiveLinkSolidAxlewithoutSteering Use the Five Link Solid Axle without steering suspension template.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-