SeatBeltAnchorageBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
SeatBeltAnchorageBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.VehicleDesign.SeatBeltAnchorage
builderTo create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateSeatBeltAnchorageBuilder
Default values.
Property Value AnchorageLocation VehicleStructure BackAngleDbl 22 BackAngleDim.Value 22 BeltRouting OutsideSeatThruSeatSpring FloorHeightDim.Value 325 (millimeters part), 12.8 (inches part) SeatPosition Left SeatType MovableFront SgrpXvalDim.Value 1500 (millimeters part), 59.06 (inches part) SgrpYvalDim.Value -400 (millimeters part), -15.75 (inches part) SgrpZvalDim.Value 650 (millimeters part), 25.59 (inches part) Standard J383SeatBeltAnchorage New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AnchorageLocation | Returns or sets the anchorage location type |
BackAngleDbl | Returns or sets the value of back angle |
BackAngleDim | Returns the dimension expression for back angle |
BeltRouting | Returns or sets the belt routing type |
FloorHeightDim | Returns the dimension expression for floor height |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SeatPosition | Returns or sets the seat position type |
SeatType | Returns or sets the seat type |
SgrpPoint | Returns or sets the SgRp point |
SgrpXvalDim | Returns the dimension expression for the X coordinate of SgRp |
SgrpYvalDim | Returns the dimension expression for the Y coordinate of SgRp |
SgrpZvalDim | Returns the dimension expression for the Z coordinate of SgRp |
Standard | Returns or sets the standard for seat belt anchorage |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
J1369Illu | Shows an illustration picture for standard j1369 |
J383Illu | Shows an illustration picture for standard j383 |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SeatBeltAnchorageBuilderAnchorageLocationTypes Enumeration | the seat belt anchorage location type |
SeatBeltAnchorageBuilderRoutingTypes Enumeration | the seat belt routing type |
SeatBeltAnchorageBuilderSeatPositionTypes Enumeration | the seat position type |
SeatBeltAnchorageBuilderSeatTypes Enumeration | the seat type |
SeatBeltAnchorageBuilderStandardTypes Enumeration | the standard type |
Property Detail¶
AnchorageLocation¶
-
SeatBeltAnchorageBuilder.
AnchorageLocation
¶ Returns or sets the anchorage location type
-------------------------------------
Getter Method
Signature
AnchorageLocation()
Returns: Return type: NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilderAnchorageLocationTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnchorageLocation(anchorageLocation)
Parameters: anchorageLocation ( NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilderAnchorageLocationTypes
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
BackAngleDbl¶
-
SeatBeltAnchorageBuilder.
BackAngleDbl
¶ Returns or sets the value of back angle
-------------------------------------
Getter Method
Signature
BackAngleDbl()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BackAngleDbl(backAngleDbl)
Parameters: backAngleDbl (float) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
BackAngleDim¶
-
SeatBeltAnchorageBuilder.
BackAngleDim
¶ Returns the dimension expression for back angle
-------------------------------------
Getter Method
Signature
BackAngleDim()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
BeltRouting¶
-
SeatBeltAnchorageBuilder.
BeltRouting
¶ Returns or sets the belt routing type
-------------------------------------
Getter Method
Signature
BeltRouting()
Returns: Return type: NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilderRoutingTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BeltRouting(beltRouting)
Parameters: beltRouting ( NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilderRoutingTypes
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
FloorHeightDim¶
-
SeatBeltAnchorageBuilder.
FloorHeightDim
¶ Returns the dimension expression for floor height
-------------------------------------
Getter Method
Signature
FloorHeightDim()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
SeatPosition¶
-
SeatBeltAnchorageBuilder.
SeatPosition
¶ Returns or sets the seat position type
-------------------------------------
Getter Method
Signature
SeatPosition()
Returns: Return type: NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilderSeatPositionTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeatPosition(seatPosition)
Parameters: seatPosition ( NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilderSeatPositionTypes
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SeatType¶
-
SeatBeltAnchorageBuilder.
SeatType
¶ Returns or sets the seat type
-------------------------------------
Getter Method
Signature
SeatType()
Returns: Return type: NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilderSeatTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeatType(seatType)
Parameters: seatType ( NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilderSeatTypes
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SgrpPoint¶
-
SeatBeltAnchorageBuilder.
SgrpPoint
¶ Returns or sets the SgRp point
-------------------------------------
Getter Method
Signature
SgrpPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SgrpPoint(sgrpPoint)
Parameters: sgrpPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SgrpXvalDim¶
-
SeatBeltAnchorageBuilder.
SgrpXvalDim
¶ Returns the dimension expression for the X coordinate of SgRp
-------------------------------------
Getter Method
Signature
SgrpXvalDim()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
SgrpYvalDim¶
-
SeatBeltAnchorageBuilder.
SgrpYvalDim
¶ Returns the dimension expression for the Y coordinate of SgRp
-------------------------------------
Getter Method
Signature
SgrpYvalDim()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
SgrpZvalDim¶
-
SeatBeltAnchorageBuilder.
SgrpZvalDim
¶ Returns the dimension expression for the Z coordinate of SgRp
-------------------------------------
Getter Method
Signature
SgrpZvalDim()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Standard¶
-
SeatBeltAnchorageBuilder.
Standard
¶ Returns or sets the standard for seat belt anchorage
-------------------------------------
Getter Method
Signature
Standard()
Returns: Return type: NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilderStandardTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Standard(standard)
Parameters: standard ( NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilderStandardTypes
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
J1369Illu¶
-
SeatBeltAnchorageBuilder.
J1369Illu
¶ Shows an illustration picture for standard j1369
Signature
J1369Illu()
New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
J383Illu¶
-
SeatBeltAnchorageBuilder.
J383Illu
¶ Shows an illustration picture for standard j383
Signature
J383Illu()
New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Validate¶
-
SeatBeltAnchorageBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.