PedestrianProtectionBuilderStandardType Enumeration¶
NXOpen.Features.VehicleDesign.PedestrianProtectionBuilder.StandardType is an alias for NXOpen.Features.VehicleDesign.PedestrianProtectionBuilderStandardType
-
class
NXOpen.Features.VehicleDesign.
PedestrianProtectionBuilderStandardType
¶ Bases:
object
Settings for the type of pedestrian protection standard to use in the study.
Enum Members
Enum Member Enum Member Description NorthAmerican North american standardEuropean European standardJapanese Japanese standardKorean Korean standardChinese Chinese standard-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-