MirrorCertificationBuilderLocationType Enumeration¶
NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.LocationType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderLocationType
-
class
NXOpen.Features.VehicleDesign.
MirrorCertificationBuilderLocationType
¶ Bases:
object
Used to indicate the mirror location.
Enum Members
Enum Member Enum Member Description Inside Represents the inside locationDriverSide Represents the driver side locationPassengerSide -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-