MirrorCertificationBuilderInstructionFieldPositionType Enumeration¶
NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.InstructionFieldPositionType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderInstructionFieldPositionType
-
class
NXOpen.Features.VehicleDesign.
MirrorCertificationBuilderInstructionFieldPositionType
¶ Bases:
object
Used to indicate the postion where the instruction field will be.
Enum Members
Enum Member Enum Member Description OnTargetWall Represents that the instrucition field is on target wallOnRoadSurface Represents that the instrucition field is on road surface-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-