MirrorCertificationBuilderInsideStandardsType Enumeration¶
NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.InsideStandardsType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderInsideStandardsType
-
class
NXOpen.Features.VehicleDesign.
MirrorCertificationBuilderInsideStandardsType
¶ Bases:
object
Used to indicate the standard for the inside mirror.
Enum Members
Enum Member Enum Member Description UsaCanadaFmvss111Cmvsss111 Represents USA - Canada : FMVSS111 - CMVSSS111 standardEurope200397EcEcer4602 Represents Europe : 2003/97/EC - ECE R46.02 standardJapanArticle44Trias29Trias39 Represents Japan : Article 44/TRIAS 29/TRIAS 39 standardAustraliaAdr1402 Represents Australia : ADR 14/02 standardSaudiArabiaGulfStatesSsa770771Gs421442 Represents Saudi Arabia - Gulf States : SSA 770/771 GS 421/442 standardChinaGb150842006 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-