ManikinBuilderStandardType Enumeration¶
NXOpen.Features.VehicleDesign.ManikinBuilder.StandardType is an alias for NXOpen.Features.VehicleDesign.ManikinBuilderStandardType
-
class
NXOpen.Features.VehicleDesign.
ManikinBuilderStandardType
¶ Bases:
object
the vehicle standard type
Enum Members
Enum Member Enum Member Description SAEJ826Jul1995 1995 SAE j826 Standard Type Saej833 SAE j833 Standard Type UserDefined User Defined Manikin Size Type SAEJ826Nov2008 2008 SAE j826 Standard Type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-